Skip to main content
sony_nix
Associate
April 29, 2017
Question

STM32F7 CAN Transmit IT Flags

  • April 29, 2017
  • 0 replies
  • 524 views
Posted on April 29, 2017 at 22:20

Hello guys,

The problem appears on CAN2 (don't know yet if it appears on CAN1 or CAN3).

I'm using HAL_CAN_Transmit_IT() to send data.

In the CAN2_TX_IRQHandler() I call HAL_CAN_IRQHandler().

Action:

1. Send 1 CAN frame on mailbox0.

Expect:

1. When the TX Interrupt is entered, the CAN_TSR register doesn't show the flags: RQCP0 and TME0 as beeing set. 

2. The 

RQCP0 and TME0 flags are set, but it seems with a pretty high delay from executing the TX Interrupt.

3. The documentation 'RM0410 -> STM32F76xxx and STM32F77xxx' specifies that the TX Interrupt is triggered when flags: RQCPx is set while TMEIE bit is enabled.

Problem:

1. Question: How does the CAN TX Interrupt gets triggered without 

RQCPx set in the CAN_TSR? 

Debugging:

1. Send one CAN frame and check the CAN_TSR for available mailboxes, after exiting the TX Interrupt. 

I found the following pattern of free mailboxes:

(each number represents tx free mailbox that is going to be used for sending the frame)

0000101010101 | 0000101010101 | 0000101010101 | 0000101010101

    This topic has been closed for replies.