Skip to main content
scott239955_stm1_stmicro_com
Associate II
March 27, 2024
Solved

STM32F7 and STM32H7 HDMI implementation

  • March 27, 2024
  • 5 replies
  • 5105 views

Hello,

Please forgive me for what is probably a newbie question.  What is required to implement an HDMI interface with the STM32F7 or H7 MCU series?  Is a DSI-to-HDMI bridge always required?  What is the max. supported display resolution?

Thanks,

Scott

This topic has been closed for replies.
Best answer by Tesla DeLorean

HDMI-CEC is an entirely different thing, and not the question being asked.

Yes, you're likely to need a bridge, you can only use two-lanes, so basically limited to 800 Mbps - 1 Gbps

So perhaps resolutions of around 1024x600, 1280x800 or 1388x768, say 1.1 Mpixel, and perhaps play games with the color depth or refresh rate to keep you under the cap.

So not going to remotely entertain FHD or UHD

rough_bw = x_res * y_res * color_depth * refresh_rate

5 replies

STTwo-32
ST Technical Moderator
March 27, 2024

Hello @scott239955_stm1_stmicro_com 

I suggest you to take a look at the HDMI-CEC chapter of the STM32H7 or STM32F7 that you are using.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
March 27, 2024

HDMI-CEC is an entirely different thing, and not the question being asked.

Yes, you're likely to need a bridge, you can only use two-lanes, so basically limited to 800 Mbps - 1 Gbps

So perhaps resolutions of around 1024x600, 1280x800 or 1388x768, say 1.1 Mpixel, and perhaps play games with the color depth or refresh rate to keep you under the cap.

So not going to remotely entertain FHD or UHD

rough_bw = x_res * y_res * color_depth * refresh_rate

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
scott239955_stm1_stmicro_com
Associate II
March 27, 2024

Thank you.  So I'm concerned that 1080p might be difficult.  We don't need high frame rates, but I don't know the color depth the UI designers are going to want.  It appears that we'd need to keep the frame rate to, say, 24 Hz and depth to 18bpp.

Also, I'm not seeing that the H7 series has a DSI interface, so is it even a candidate for HDMI video?

Scott