Question
STM32F4Discovery - external VDD supply
Posted on June 04, 2013 at 13:52
Hi All,
Is it possible to use STM32f4Discovery without powering it’s ST Link section and associated LEDs. External 5V (at P2 pin 3,4) will power up ST Link section and associated LEDs. Is it safe to remove JP1 and apply external 3.3V at VDD pin? In this case some on board devices(IC U1, U2, U3, U5, U6, U7, U8, U9) using 3V supply will not receive power. Will this have any adverse effect on STM32F407 operation (latch up, ADC performance etc)?