STM32f469 SDRAM Read/Write issue on FMC Bank2
Hello all,
I have W9816G6JH( Winbond) SDRAM interfaced with STM32f469 on a custom board.
SDRAM is interfaced on FMC Bank2.
I have generated SDRAM initialization code for MDK-ARM using CubeMx.
When I Write and Read back on SDRAM address 0xD0000000 it shows 0x00 only.
below is my SDRAM initialization code :
#define SDRAM_BANK_ADDR ((uint32_t)0xD0000000)
#define SDRAM_MEMORY_WIDTH FMC_SDRAM_MEM_BUS_WIDTH_16
#define SDCLOCK_PERIOD FMC_SDRAM_CLOCK_PERIOD_3
#define SDRAM_TIMEOUT ((uint32_t)0xFFFF)
void SDRAM_Initialize(void)
{
/*##-1- Configure the SDRAM device #########################################*/
/* SDRAM device configuration */
hsdram.Instance = FMC_SDRAM_DEVICE;
/* Timing configuration for 90 MHz of SDRAM clock frequency (180MHz/2) */
/* TMRD: 2 Clock cycles */
SDRAM_Timing.LoadToActiveDelay = 2;
/* TXSR: min=70ns (6x11.90ns) */
SDRAM_Timing.ExitSelfRefreshDelay = 7;
/* TRAS: min=42ns (4x11.90ns) max=120k (ns) */
SDRAM_Timing.SelfRefreshTime = 4;
/* TRC: min=63 (6x11.90ns) */
SDRAM_Timing.RowCycleDelay = 7;
/* TWR: 2 Clock cycles */
SDRAM_Timing.WriteRecoveryTime = 2;
/* TRP: 15ns => 2x11.90ns */
SDRAM_Timing.RPDelay = 2;
/* TRCD: 15ns => 2x11.90ns */
SDRAM_Timing.RCDDelay = 2;
hsdram.Init.SDBank = FMC_SDRAM_BANK2;
hsdram.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
hsdram.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
hsdram.Init.MemoryDataWidth = SDRAM_MEMORY_WIDTH;
hsdram.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_2;
hsdram.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
hsdram.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
hsdram.Init.SDClockPeriod = SDCLOCK_PERIOD;
hsdram.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
hsdram.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1;
/* Initialize the SDRAM controller */
if(HAL_SDRAM_Init(&hsdram, &SDRAM_Timing) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/* Program the SDRAM external device */
SDRAM_Initialization_Sequence(&hsdram, &command);
}
static void SDRAM_Initialization_Sequence (SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Command)
{
__IO uint32_t tmpmrd =0;
/* Step 3: Configure a clock configuration enable command */
Command->CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
Command->AutoRefreshNumber = 1;
Command->ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, Command, 0x1000);
/* Step 4: Insert 100 ms delay */
HAL_Delay(100);
/* Step 5: Configure a PALL (precharge all) command */
Command->CommandMode = FMC_SDRAM_CMD_PALL;
Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
Command->AutoRefreshNumber = 1;
Command->ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, Command, 0x1000);
/* Step 6 : Configure a Auto-Refresh command */
Command->CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;
Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
Command->AutoRefreshNumber = 4;
Command->ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, Command, 0x1000);
/* Step 7: Program the external memory mode register */
tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_2 |
SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL |
SDRAM_MODEREG_CAS_LATENCY_3 |
SDRAM_MODEREG_OPERATING_MODE_STANDARD |
SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;
Command->CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
Command->AutoRefreshNumber = 1;
Command->ModeRegisterDefinition = tmpmrd;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, Command, 0x1000);
/* Step 8: Set the refresh rate counter */
/* (15.62 us x Freq) - 20 */
/* Set the device refresh counter */
HAL_SDRAM_ProgramRefreshRate(hsdram, REFRESH_COUNT);
}
Below is SDRAM Read/Write Check:
uint32_t SDRAM_RWTest(void)
{
uint32_t lu32_Indx = 0;
uint32_t lu32_RWStatus = 0;
/* Fill the buffer to write */
memset(gu32_TxBuffer, 0, sizeof(gu32_RxBuffer));
memset(gu32_RxBuffer, 0, sizeof(gu32_RxBuffer));
SDRAM_FillBuffer(gu32_TxBuffer, BUFFER_SIZE, 0x0);
/* Write data to the SDRAM memory */
for (lu32_Indx = 0; lu32_Indx < BUFFER_SIZE; lu32_Indx++)
{
*(__IO uint32_t*) (SDRAM_BANK_ADDR + WRITE_READ_ADDR + 4*lu32_Indx) = gu32_TxBuffer[lu32_Indx];
}
/* Read back data from the SDRAM memory */
for (lu32_Indx = 0; lu32_Indx < BUFFER_SIZE; lu32_Indx++)
{
gu32_RxBuffer[lu32_Indx] = *(__IO uint32_t*) (SDRAM_BANK_ADDR + WRITE_READ_ADDR + 4*lu32_Indx);
}
/* Checking data integrity */
for (lu32_Indx = 0; (lu32_Indx < BUFFER_SIZE) && (lu32_RWStatus == 0); lu32_Indx++)
{
if (gu32_RxBuffer[lu32_Indx] != gu32_TxBuffer[lu32_Indx])
{
lu32_RWStatus++;
}
}
return lu32_RWStatus;
}
Does any body have interfaced SDRAM on Bank2?