Skip to main content
jameslenvo
Associate II
March 23, 2020
Question

STM32F469 CAN Rx Issues

  • March 23, 2020
  • 0 replies
  • 486 views

Hello, I am attempting to transmit a simple CAN message between two STM32F469I discovery boards.

I am using the official STM32F4 github as reference found here:

https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM324x9I_EVAL/Examples/CAN/CAN_Networking

I can get Tx working on both boards, but the receiving of messages is not working. Am I handling the receive FIFO incorrectly? I've tried different filter settings and the loopback examples works fine.

Below is my code on both boards. Appreciate any help.

 HAL_Init();
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_CAN1_Init();
 
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_4, GPIO_PIN_SET);
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_5, GPIO_PIN_SET);
 HAL_GPIO_WritePin(GPIOG, GPIO_PIN_6, GPIO_PIN_SET);
 HAL_GPIO_WritePin(GPIOK, GPIO_PIN_3, GPIO_PIN_SET);
 
 CAN1_filterConfig();
 CAN1_start();
 
 // Activate Notifcation
 // CAN1_activateNotificaiton();
 
 // Set Transmit 
 myTxMessage.StdId = SendingId;
 myTxMessage.ExtId = ReceivingId;
 myTxMessage.RTR = CAN_RTR_DATA;
 myTxMessage.IDE = CAN_ID_STD;
 myTxMessage.DLC = 2;
 myTxMessage.TransmitGlobalTime = DISABLE;
 TxData[0] = 0xAD;
 TxData[1] = 0xAD;
 
 
 ThisId = SendingId;
 // ThisId = ReceivingId;
 
 while (1) {
	 if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_0) == GPIO_PIN_SET){
 if(ThisId==SendingId){
// Lines for sending:
 if (HAL_CAN_GetTxMailbox0FreeLevel(&hcan1) != 0) {
 // Updated LED
 if(payload == 2) payload=0;
 LED_Switch(++payload);
 sendMessageStatus = HAL_CAN_AddTxMessage(&hcan1, &myTxMessage, TxData, mailbox);
 if(sendMessageStatus!=HAL_OK) {
 Error_Handler_Custom(sendMessageStatus);
 }
 } else {
 LED_Switch(3);
 }
 } else {
 /*##-5- Start the Reception process ########################################*/
 // Following lines are for receiving
 if(payload == 2) payload=0;
 LED_Switch(++payload);
 checkFillLevelStatus = HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_RX_FIFO0);
 if(checkFillLevelStatus == 0) {
 /* Reception Missing */
 Error_Handler_Custom(HAL_TIMEOUT);
 } else {
 getMessageStatus = HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &myRxMessage, RxData);
 if(getMessageStatus != HAL_OK) {
 /* Reception Error */
 Error_Handler_Custom(getMessageStatus);
 } else if((myRxMessage.StdId != SendingId) ||
 (myRxMessage.RTR != CAN_RTR_DATA) ||
 (myRxMessage.IDE != CAN_ID_STD) ||
 (myRxMessage.DLC != 2) ||
 ((RxData[0]<<8 | RxData[1]) != 0xADAD)) {
 /* Rx message Error */
 Error_Handler_Custom(HAL_BUSY);
 } else {
 LED_Switch(3);
 }
 }
 }
		 HAL_Delay(200);
	 }
 }
}
 
static void MX_CAN1_Init(void)
{
 
 hcan1.Instance = CAN1;
 hcan1.Init.Prescaler = 2;
 hcan1.Init.Mode = CAN_MODE_NORMAL;
 hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
 hcan1.Init.TimeTriggeredMode = DISABLE;
 hcan1.Init.AutoBusOff = DISABLE;
 hcan1.Init.AutoWakeUp = DISABLE;
 hcan1.Init.AutoRetransmission = DISABLE;
 hcan1.Init.ReceiveFifoLocked = DISABLE;
 hcan1.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
 
void CAN1_filterConfig(void)
{
	CAN_FilterTypeDef filterConfig;
	filterConfig.FilterBank = 0;
 filterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
 filterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
 filterConfig.FilterIdHigh = 0x1fff;
	filterConfig.FilterIdLow = 0xffff;
 filterConfig.FilterMaskIdHigh = 0x0000;
	filterConfig.FilterMaskIdLow = 0x0000;
 filterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
	filterConfig.FilterActivation = ENABLE;
 filterConfig.SlaveStartFilterBank = 14;
 
 can1filterConfigStatus = HAL_CAN_ConfigFilter(&hcan1, &filterConfig);
 if(can1filterConfigStatus != HAL_OK)
 {
 Error_Handler_Custom(can1filterConfigStatus);
 }
}
 
uint32_t HAL_CAN_GetTxMailbox0FreeLevel(CAN_HandleTypeDef *hcan)
{
 uint32_t freelevel = 0U;
 HAL_CAN_StateTypeDef state = hcan->State;
 
 if ((state == HAL_CAN_STATE_READY) ||
 (state == HAL_CAN_STATE_LISTENING))
 {
 /* Check Tx Mailbox 0 status */
 if ((hcan->Instance->TSR & CAN_TSR_TME0) != 0U)
 {
 freelevel++;
 }
 }
 
 /* Return Tx Mailboxes free level */
 return freelevel;
}

This topic has been closed for replies.