Question
STM32F446RET6 Nokia5110
- 2 replies
- 873 views
I am using CMSIS for STM32F446RET6 (clock speed at 180 MHz) to drive Nokia5110 LCD Module via SPI1. But, this program doesn't work. When I test with STM32F103C8T6 (using CMSIS and Clock speed 72 MHz), Nokia5110 work well. Please help me. How to correct program for STM32F446RET6? Project file is attached and anyone can see connection diagram in readme file. This project is created with STM32CubeIDE 1.15.1
Edit: I have attached two files.
STM32F103C8T6_spi1_nokia5110.tar.xz is working. But, STM3F446RET6_spi1_nokia5110 not.