STM32F446RE Timer Interrupt and UART Interrupt Doesn't Work With Each Other.
I have Timer 2 interrupt and an UART 4 interrupt for reading from a GPS module. But they don't work with each other. When I disable Timer 2 interrupt UART 4 interrupt starts to work.
I did set Timer 2 interrupt preemption priority to 1 and UART 4 interrupt preemption priority to 0. And nothing changed.
If I understood it correctly it looks like Timer interrupt is so fast and distrupts the UART interrupt. But again If I understood it correctly with preemption priority settings software shouldn't call Timer interrupt when in UART interrupt because UART interrupt has a priority. What I'm doing wrong in here? Thank you for reading.