Question
STM32F446RE can no connect to target
Posted on November 17, 2015 at 14:59
Hello, this is my first post.
It is the first time I use an STM32 Device, I am familiar with 32Bit processors of TI so far.I did a new PCB connected with the ST-Link programmer of a Nucleo board. But I can not connect to my board. I am using the STM32 St-Link Utility.My configuration:TQFP64Pin 19,32,48,64,13,1 on 3V3Pin 31, 47, 18, 63, 12 on GNDPin 30 on 4.7uF to GND (VCAP)25 MHz crystal on Pin 5 & 6Pin 60 (Boot0) connected to 10k to GNDPin 46 to ST-Programmer SWDPin 49 to ST-Programmer CLK Pin 7 to ST-Programmer NRSTThe programmer also has GND of the board.All other Pins are left floating.Power consumption 0.3 mA! The CPU seems not to run.Pin 1 is at the lower left if the text on the chip is readable.The voltage on the VCap_0 is 0V.It is a bit confusing, I just have seen that the VCAP_1 (Pin 30) capacitor is not populated and has been shorted to ground on the Nucleo board.Could anyone give me an advice how to handle this situation?Thanks in advanceChris