Question
STM32F439 Issue with CAN Recieve using both FIFOs
Posted on February 06, 2018 at 20:17
Hi,
I have a weird issue happening in my code related to CAN Receive. I have 2 filters set up to each pass a single Message:
void FilterSetup(void)
{ CAN_FilterConfTypeDef sFilterConfig;uint32_t EXTID = 0x0CF0040A;
sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = (EXTID >> 13) & 0xFFFF; sFilterConfig.FilterIdLow = ((EXTID << 3) & 0xFFF8) | 4; sFilterConfig.FilterMaskIdHigh = 0xFFFF; sFilterConfig.FilterMaskIdLow = 0xFFFC; sFilterConfig.FilterFIFOAssignment = CAN_FIFO0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 9;if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{ Error_Handler(); }uint32_t EXTID1 = 0x18F003F8;
sFilterConfig.FilterNumber = 1;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = (EXTID1 >> 13) & 0xFFFF; sFilterConfig.FilterIdLow = ((EXTID1 << 3) & 0xFFF8) | 4; sFilterConfig.FilterMaskIdHigh = 0xFFFF; sFilterConfig.FilterMaskIdLow = 0xFFFC; sFilterConfig.FilterFIFOAssignment = CAN_FIFO1; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 10;if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{ Error_Handler(); }}When I run my code I see the following behavior:
- Using a PCAN tool, I send my 0x18F003F8 message to the MCU. This works fine and i see the message was received in FIFO1.
- Using a PCAN tool, I send my 0x0CF0040A message to the MCU. This also works fine and I see the message received in FIFO0.
- If I send 0x0CF0040A first (receives in FIFO0) then send 0x18F003F8. Until I reset the MCU, 0x18F003F8 is still received but on FIFO0 not FIFO1.
Any thoughts on how this might be occurring? I am using the STM32Cube_FW_F4_V1.18.0 Drivers.
Thanks,
Sean