Question
STM32F439 incorrect NAND ID read
Posted on January 23, 2014 at 08:08
Hello,
I'm using a STM32F439 with the MT29F2G08 NAND from Micron. When I read the NAND ID on Address 0x20, I receive the correct ONFI codes. When I Read the ID on address 0x00, I read the correct Maker ID, but the following bytes are incorrect. I expect the following Byte values: Byte0 should be 0x2C and i read also 0x2C. That one is fine Byte1 should be 0xDA and i read 0x01 Byte2 should be 0x90 and i read 0x02 Byte3 should be 0x95 and i read 0x03 Byte4 should be 0x86 and i read 0x00 Does anybody have the same problem before?