Skip to main content
gajraj
Associate
July 28, 2016
Question

STM32F439 - FMC interfacing SDRAM, NVRAM and ARNIC 429

Posted on July 28, 2016 at 07:53

Hi,

We are developing a display using STM32F439NIH6 Microcontroller in our design.  We have the following technical queries:

We have referred to your evaluation board design and we are interfacing STM32F439NIH6 with SDRAM, NVRAM and ARINC 429 devices through FMC data bus and Address bus.

Can we connect all 3 loads and access simultaneously.

We are unable to drive all the three loads. During the process of analysis we came across I/O Cell Compensation in Reference Manual. 

Is this can be enabled for FMC?

We are working on 3.3V supply and configured the System Clock as 180MHz.

We tried to enable I/O cell compensation by reducing the System Clock to 100 MHz/90 MHz and 50 MHz.

We are unable to enable the Cell Compensation. Please help us in this regard by providing the procedure to enable the same.

#stm32f439
This topic has been closed for replies.

1 reply

Associate II
August 30, 2024

ARINC 429 Interface with STM32 MCU - Help Needed

Dear gajraj,

I hope this message finds you well.

I recently saw your post about interfacing an STM32F439NIH6 with ARINC 429 using the HI-3585 transceiver. I'm currently working on a project that requires a similar interface with an STM32 MCU and HI-3585.

As this is my first experience with ARINC 429, I'm encountering some challenges during configuration. I would be grateful if you could offer any guidance or advice to help me understand and overcome these issues.

Thank you for your time and consideration.