Skip to main content
John Hite
Associate III
Jan 12, 2017 9:36 PM UTC
Solved

stm32f437xx.h

Posted on January 12, 2017 at 22:36

Where can one find the current version of stm32f437xx.h?

Thanks,

jh

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Jan 13, 2017 9:37 PM UTC
    Posted on January 13, 2017 at 21:37

    You are mixing include and source files front two different libraries, and that's not going to work at all well

    You want to match stm32f437xx.h with 

    stm32f4xx_hal_gpio.c, not stm32f4xx_gpio.c

    STM32Cube_FW_F4_V1.9.0\Drivers\CMSIS\Device\ST\STM32F4xx\Include\stm32f437xx.h

    STM32Cube_FW_F4_V1.9.0\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_gpio.c

    OR

    STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Libraries\CMSIS\Device\ST\STM32F4xx\Include\stm32f4xx.h

    STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Libraries\STM32F4xx_StdPeriph_Driver\src\stm32f4xx_gpio.c

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    6 replies

    Tesla DeLorean
    Guru
    Jan 12, 2017 9:47 PM UTC
    Posted on January 12, 2017 at 22:47

    Where did the one you have come from?

    The SPL you define the model and it pulls the appropriate structures from stm32f4xx.h

    #define STM32F427_437xx

    STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Libraries\CMSIS\Device\ST\STM32F4xx\Include\stm32f4xx.h

    Under Cube

    STM32Cube_FW_F4_V1.9.0\Drivers\CMSIS\Device\ST\STM32F4xx\Include\stm32f446xx.h

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    John Hite
    John HiteAuthor
    Associate III
    Jan 12, 2017 11:16 PM UTC
    Posted on January 12, 2017 at 23:16

     ,

     ,

    The current version came from svn for a previous version of the project.

    What is this model that is to be defined? In what file do I place the statement

    ♯ define STM32F427_437xx

     ,

    ?

    We are not using HAL or CMSIS and therefore not using Cube.

    Thanks,

    jh

    Tesla DeLorean
    Guru
    Jan 13, 2017 1:55 AM UTC
    Posted on January 13, 2017 at 01:55

    For the SPL I typically pass it as a command line define for the compiler.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..