Skip to main content
kyrin
Associate
May 12, 2021 9:46 AM UTC
Solved

STM32F437AIH6 UBGA-169 missing FMC_A13 ,how to add extension SRAM ?

1�?I have choose STM32F437AIH6 , and want to add an extension SRAM , but MCU missing PIN FMC_A13,In this condition , is it feasible to use SRAM?

2�?Use Trace Macrocell function,but FMC_A19 and TRACE0 are the same pin . is it affect to code coverage test (Trace Macrocell) if i want use FMC_A19 to acess extersion SRAM?

thanks

kyrin

This topic has been closed for replies.
PMath.4
PMath.4Best answer
Senior III
May 13, 2021 8:41 AM UTC

If you must use SRAM rather than SDRAM then connect A13 of the RAM either high or low. You will use half the available memory but the remaining half should work

4 replies

Tesla DeLorean
Guru
May 12, 2021 12:01 PM UTC

Right, you're likely going to have to make a choice between full bus external memory and trace capability. You should be able to use a subset of the memory.

Most have migrated to SDRAM due to costs

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
kyrin
kyrinAuthor
Associate
May 13, 2021 2:40 AM UTC

Thank you to reply . Do you have any idea about question 1 ?

PMath.4
PMath.4Best answer
Senior III
May 13, 2021 8:41 AM UTC

If you must use SRAM rather than SDRAM then connect A13 of the RAM either high or low. You will use half the available memory but the remaining half should work

kyrin
kyrinAuthor
Associate
May 14, 2021 7:03 AM UTC

thanks .got it.