Skip to main content
slawek
Associate III
January 28, 2020
Question

STM32F429ZI Flash Problem. MCU sets FLASH->SR bits: PGPERR and PGSERR all the time even it is cleared just before.

  • January 28, 2020
  • 3 replies
  • 1267 views

MCU sets FLASH->SR bits: PGPERR and PGSERR all the time even immediately after it is cleared.

It causes a problem with erasing flash memory.

I am using RTOS(TIM1 as a base), Timers and Systick as well but I think those shouldn't be a problem.

Code is executed from flash but from different regions, so it isn't overlapping.

I was thinking if cache can make this problem, but after turning of cache before I have still the problem.

I was doing flashing other sectors on STM32F1 and there was no problems with it, but if I remember correctly there are no such flags.

This topic has been closed for replies.

3 replies

berendi
Principal
January 28, 2020

I suspect there is a corrupted or uninitialized pointer somewhere that tries to write the flash.

If it's a null pointer, you can catch it by mapping RAM at address 0, see SYSCFG->MEMRMP. Move the beginning of the RAM up by a few words in the linker script, place some guard value at 0x20000000, and see if it changes.

jwoerle
Associate II
May 29, 2020

Thanks for sharing this answer. This thread and the following thread solved a similar issue of me:

https://community.st.com/s/question/0D50X00009XkWriSAF/stm32f407-flash-programming-error-pgserr-and-pgperr

It was actually a bug introduced by me:

I have a watchdog running and reset it frequently with

HAL_IWDG_Refresh(&hiwdg);

 For debugging purpose, I disable my watchdog init

// disable for debugging purpose
// MX_IWDG_Init();

 This causes problem in the Flash interface, where the FLASH_WaitForLastOperation() function fails.

My solution is to also disable the HAL_IWDG_Refresh() function in debugging.

slawek
slawekAuthor
Associate III
January 28, 2020

The clue seems to be good. I had no time to do exactly what you mentioned yet, but I turned off some tasks and I think the guilty one is default task with LWIP initialization (because it looks that it helped). I would need to investigate more because I would need to have both Ethernet and Flashing at same time.