Skip to main content
Tesla DeLorean
Guru
October 17, 2013
Question

STM32F429I-DISCO SDRAM Initialization in system_stm32f4xx.c

  • October 17, 2013
  • 3 replies
  • 1304 views
Posted on October 17, 2013 at 21:31

The code shipped in the FW library either says it's not implemented, or is in fact the code for the STM324x9I-EVAL with or without the name changed. The code was for Bank1 SDRAM at 0xC0000000, it will not work with the different part at Bank2 0xD0000000 on the STM32F429I-DISCO board!!

#ifdef DATA_IN_ExtSDRAM
/**
* @brief Setup the external memory controller.
* Called in startup_stm32f429_439xx.s before jump to main.
* This function configures the external SDRAM mounted on STM32F429I-DISCO board
* This SDRAM will be used as program data memory (including heap and stack).
* @param None
* @retval None
*/
void SystemInit_ExtMemCtl(void)
{
/* This function will be implemented in next versions */
}
#endif /* DATA_IN_ExtSDRAM */

This annoyed me, so I fixed it. This now allows SystemInit() to bring up the SDRAM, and for it to be used by the C Run-time library code. If this helps you, please send your appreciation.

https://docs.google.com/file/d/0B7OY5pub_GfISU9vOTlZa3ItMDQ/edit?usp=sharing

#this-annoyed-me #so-i-fixed-it
    This topic has been closed for replies.

    3 replies

    orders-st
    Associate
    January 8, 2014
    Posted on January 08, 2014 at 22:05

    This is AWESOME Clive. I will use this in my startup scripts for my ST32F4 design.

    Mark Edwards
    Associate III
    January 11, 2014
    Posted on January 11, 2014 at 03:00

    I wondered why the included method didn't work for me and assumed I had done something wrong.

    Here is my quick and dirty method… (called from main). OK, so not optimised to run at 180MHz (I presume it’s designed to run at 168MHz). Also some interesting differences i.e. why the extra bits in GPIOB->MODER when only PB5&6 used (on the 429 Discovery board)?

    /*----------------------------------------------------------------------------
    SDRAM Initialisation - 4194304 Bytes
    *----------------------------------------------------------------------------*/
    void SDRAM_Init (void) {
    uint32_t temp32;
    // GPIOB Configuration - PB.6&5
    GPIOB->MODER = GPIOB->MODER | 0x2800; // Alt Fn
    GPIOB->OSPEEDR = GPIOB->OSPEEDR | 0x2800; // 50MHz
    GPIOB->AFR[0] = GPIOB->AFR[0] | 0x0CC00000; // SDRAM
    // GPIOC Configuration - PC.0
    GPIOC->MODER = GPIOC->MODER | 0x2; // Alt Fn
    GPIOC->OSPEEDR = GPIOC->OSPEEDR | 0x2; // 50MHz
    GPIOC->AFR[0] = GPIOC->AFR[0] | 0xC; // SDRAM
    // GPIOD Configuration - PD.15,14,10,9,8,1,0
    GPIOD->MODER = GPIOD->MODER | 0xA02A000A; // Alt Fn
    GPIOD->OSPEEDR = GPIOD->OSPEEDR | 0xA02A000A; // 50MHz
    GPIOD->AFR[0] = GPIOD->AFR[0] | 0xCC; // SDRAM AFRL
    GPIOD->AFR[1] = GPIOD->AFR[1] | 0xCC000CCC; // SDRAM AFRH
    // GPIOE Configuration - PE.15,14,13,12,11,10,9,8,7,1,0
    GPIOE->MODER = GPIOE->MODER | 0xAAAA800A; // Alt Fn
    GPIOE->OSPEEDR = GPIOE->OSPEEDR | 0xAAAA800A; // 50MHz
    GPIOE->AFR[0] = GPIOE->AFR[0] | 0xC00000CC; // SDRAM AFRL
    GPIOE->AFR[1] = GPIOE->AFR[1] | 0xCCCCCCCC; // SDRAM AFRH
    // GPIOF Configuration - PE.15,14,13,12,11,5,4,3,2,1,0
    GPIOF->MODER = GPIOF->MODER | 0xAA800AAA; // Alt Fn
    GPIOF->OSPEEDR = GPIOF->OSPEEDR | 0xAA800AAA; // 50MHz
    GPIOF->AFR[0] = GPIOF->AFR[0] | 0xCCCCCC; // SDRAM AFRL
    GPIOF->AFR[1] = GPIOF->AFR[1] | 0xCCCCC000; // SDRAM AFRH
    // GPIOG Configuration - PG.15,8,5,4,1,0
    GPIOG->MODER = GPIOG->MODER | 0x80020A0A; // Alt Fn
    GPIOG->OSPEEDR = GPIOG->OSPEEDR | 0x80020A0A; // 50MHz
    GPIOG->AFR[0] = GPIOG->AFR[0] | 0xCC00CC; // SDRAM AFRL
    GPIOG->AFR[1] = GPIOG->AFR[1] | 0xC000000C; // SDRAM AFRH
    // Enable Peripheral Clock
    RCC->AHB3ENR = RCC->AHB3ENR | 0x1; // Enable FMC
    // FMC SDRAM bank initialization
    FMC_Bank5_6->SDCR[0] = 0x2800;
    FMC_Bank5_6->SDCR[1] = 0x1D4;
    FMC_Bank5_6->SDTR[0] = 0x106000;
    FMC_Bank5_6->SDTR[1] = 0x10361;
    // FMC SDRAM device initialisation sequence 
    // Configure a clock configuration enable command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x9; // Send Command
    //need 100ms delay
    for (temp32 = 0x00; temp32 < 
    0xD0000
    ; temp32++) {
    }
    // PALL (precharge all) command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0xA; // Send Command
    // Auto-Refresh command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x6B; // Send First Command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x6B; // Send Second Command
    // Load Mode Register command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x4620C; // Send Command
    // Set the refresh rate counter
    FMC_Bank5_6->SDRTR = 0x556;
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    /* Disable write protection */
    temp32 = FMC_Bank5_6->SDCR[0]; 
    FMC_Bank5_6->SDCR[0] = (temp32 & 0xFFFFFDFF);
    }

    Tesla DeLorean
    Guru
    January 11, 2014
    Posted on January 11, 2014 at 07:17

    The GPIOB stuff related to post Reset defaults for register, and modified STM324x9I-EVAL code to work on second bank. Had tested memory against this, but will revisit.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..