Skip to main content
marabini
Visitor II
October 4, 2016
Question

STM32F429i-Disco GPIO reset state

  • October 4, 2016
  • 1 reply
  • 586 views
Posted on October 04, 2016 at 11:17

Hello,

I've a problem with the reset pushbutton state in the STM32F429i-DISCO: when I push the button I see that some pins are not in the three-state but are pulled down even if there are no other logic that make this work (pin PG5).

Another problem is that when I release the reset pushbutton, I see that the pins are pulled down until the FW takes the control. They are not in three-state status.

Thanks.

 
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    October 4, 2016
    Posted on October 04, 2016 at 18:13

    PG5 connects to the SDRAM, what is that specified to do? The SDRAM also doesn't have an asynchronous reset connection.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..