STM32F429 TIM1 trigger flag (TIF) issue
I have TIM1 configured in one pulse mode triggered by rising edge on TIM1_CH1 to generate single pulse. Timer works correctly (generate single pulse for each rising edge on input). Datasheet claims that TIF flag is set on trigger event in all modes but gated mode. In gated mode flag is set when timer starts and also when stops. I am running timer in trigger mode but flag is rised when trigger event and also when timer stops. Like in gated mode. Looks like a bug. Has anyone observed this problem as well?