Skip to main content
FLast.5
Associate II
Jan 11, 2021 1:36 PM UTC
Solved

STM32F429 SPI pins die out after working for some time. Is it hardware problem or software problem ?

0

I am working with SPI on STM32F429 to write data on MX25V1006F flash memory. I am not using cubeMX library.

My problem is that it works for a while and then suddenly it doesn't work. I have replaced MCU several times but I faced same problem again and again. When checking the internal protection diode on SPI pins (0.8V or short), the measurements are different from good MCU SPI pins (0.6V). Could it be hardware problem or software problem. I am connecting the MOSI and MISO pins directly to flash MISO and MOSI pins respectively with no resistors in between. Could this be the reason for SPI pins dying out ?

As I understand SPI pins doesn't need pull up. By referring to internet sources, I connected MISO pins with 3.3K pull up but there is no change.

I reduced SPI data speed but I get same problem.

I checked the waveforms on SPI, and there is no waveform at all on one STM32F429 MCU and only SCK waveform with no MOSI change on another STM32F429 MCU. I suspect this is a hardware problem but I am unable to trace it. In my board, there is no other codes or functions conflicting in SPI1 (PortB 3,4,5)

Here is my SPI code

void SPI_Flash_Port_Init(void) 
{ 
 SPI_InitTypeDef SPI_InitStruct; 
 GPIO_InitTypeDef GPIO_InitStructure;
 
 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); 
 
 // spi1 cs setting
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
 
 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_Init(GPIOB, &GPIO_InitStructure); // Name: EX_IO1 -> CS
 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_Init(GPIOB, &GPIO_InitStructure); // I2C2_SDA -> Flash WP, HOLD
 
 // spi1 miso, mosi, sck setting
 RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1,ENABLE); // APB2CLK = 84Mhz, APB2Timer = 168Mhz
 
 GPIO_PinAFConfig(SPI1_SCL_Port, GPIO_PinSource3, GPIO_AF_SPI1);
 GPIO_PinAFConfig(SPI1_MISO_Port, GPIO_PinSource4, GPIO_AF_SPI1);
 GPIO_PinAFConfig(SPI1_MOSI_Port, GPIO_PinSource5, GPIO_AF_SPI1);
 
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
 
 GPIO_InitStructure.GPIO_Pin = SPI1_SCL_Pin; GPIO_Init(SPI1_SCL_Port, &GPIO_InitStructure);
 GPIO_InitStructure.GPIO_Pin = SPI1_MISO_Pin; GPIO_Init(SPI1_MISO_Port, &GPIO_InitStructure);
 GPIO_InitStructure.GPIO_Pin = SPI1_MOSI_Pin; GPIO_Init(SPI1_MOSI_Port, &GPIO_InitStructure);
 
 
 SPI_I2S_DeInit(SPI1);
 SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; 
 SPI_InitStruct.SPI_Mode = SPI_Mode_Master; 
 SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; 
 SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; 
 SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
 SPI_InitStruct.SPI_NSS = SPI_NSS_Soft; 
 SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256;
 // SPI_BaudRatePrescaler_2 // clk = 84 / 2 = 42.0 Mhz
 // SPI_BaudRatePrescaler_4 // clk = 84 / 4 = 21.0 Mhz
 // SPI_BaudRatePrescaler_8 // clk = 84 / 8 = 10.5 Mhz
 // SPI_BaudRatePrescaler_16 // clk = 84 / 16 = 5.2 Mhz
 // SPI_BaudRatePrescaler_32 // clk = 84 / 32 = 2.6 Mhz
 // SPI_BaudRatePrescaler_64 // clk = 84 / 64 = 1.3 Mhz
 // SPI_BaudRatePrescaler_128 // clk = 84 / 128 = 0.6 Mhz
 // SPI_BaudRatePrescaler_256 // clk = 84 / 256 = 0.3 Mhz 
 SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; 
 SPI_InitStruct.SPI_CRCPolynomial = 7; 
 
 SPI_Init(SPI1, &SPI_InitStruct);
 
 SPI_Cmd(SPI1, ENABLE); 
 
 EX_IO1(1); // CS high
 GPIO_SetBits(IIC2_SDA_Port, IIC2_SDA_Pin); // WP/Hold always high
}
 
void Flash_Spi_SendByte(unsigned char byte_value)
{
 while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET){}; SPI_I2S_SendData(SPI1,byte_value); 
 while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET){}; SPI_I2S_ReceiveData(SPI1); // Dummy rx
}
 
void Flash_Spi_ReadByte(unsigned int byte_count)
{
 unsigned int i;
 
 for(i = 0; i < byte_count; i++)
 { 
 Delay_us(5);
 SPI_Buffer[i] = 0;
 while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET){}; SPI_I2S_SendData(SPI1,0); //dummy tx
 while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET){}; SPI_Buffer[i] = SPI_I2S_ReceiveData(SPI1);
 }
}
 
#define EX_IO1(x) x ? GPIO_SetBits(GPIOB, GPIO_Pin_8) : GPIO_ResetBits(GPIOB, GPIO_Pin_8)
 
void Flash_Spi_CS(uint8_t value)
{
 Delay_us(5);
 EX_IO1(value);
 Delay_us(5);
}
 
uint8_t Flash_Spi_ID_READ(unsigned char byte_count) // read a byte 
{ 
 Flash_Spi_CS(0); // CS = 0
 Flash_Spi_SendByte(FLASH_CMD_RDID);
 Delay_us(10);
 Flash_Spi_ReadByte(byte_count); 
 Flash_Spi_CS(1); // CS = 1
 
 //Uart1_Printf("Chip ID READ\n"); 
 return true;
}

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jan 11, 2021 2:05 PM UTC

Likely a hardware problem.

I'd review grounding and power supply arrangement.

JW

1 reply

waclawek.jan
waclawek.janBest answer
Super User
Jan 11, 2021 2:05 PM UTC

Likely a hardware problem.

I'd review grounding and power supply arrangement.

JW