Skip to main content
oleg239955_st
Associate II
October 4, 2015
Question

STM32F429 SDRAM and FMC/LTDC/DMA2D priorities

  • October 4, 2015
  • 1 reply
  • 1230 views
Posted on October 04, 2015 at 15:16

Hello!

I'm trying to run STemWin/FreeRTOS/HAL on STM32F429IG revision Y at 168MHz.

SDRAM (IS42S16400J-7TLI) connected to FMC controller and runs fine by itself (CAS_LATENCY_3/CLOCK_PERIOD_2/RBURST_ENABLE/RPIPE_DELAY_1).

TFT display (AT070TN92, 800x600 RGB888) connected to LTDC and framebuffer set to SDRAM addresses. TFT clock is 24MHz. With my parameters set to LDTC I can see ~42Hz on VSYNC pin. Frame buffer addresses is 0xd0000000 and 0xd0200000.

OK, forget for now about STemWin, just configure layers and place some data to framebuffer.

ARGB888/ARGB8888 - lost sync

RGB888/ARGB8888 - runs fine.

OK, now I will modify framebuffer contents in main() loop while looking on screen.

ARGB8888/ARGB8888 - lost sync

RGB888/ARGB8888 - lost sync

RGB888/RGB888 - lost sync

RGB888/RGB565 - runs fine...

What? Why writing to SDRAM by CPU breaks LTDC DMA transfers??

OK, let's try to write to framebuffer with DMA2D.

ARGB8888/ARGB8888 - lost sync

RGB888/ARGB8888 - lost sync

RGB888/RGB888 - lost sync

RGB888/RGB565 - lost sync

RGB565/RGB565 - runs fine...

It is going even worse than CPU.

If I turn on STemWin with DMA2D transfers in LCD_DEVFUNC_FILLRECT, I can run only one layer of RGB565.

As I understand, DMA2D tries to copy to SDRAM and LTDC cannot get data from SDRAM when needed to paint next line and then sync losts. I can see it as chaotically shifting image to right/left.

What should I do with this? Can I set highest priority to LTDC transfers, so DMA2D and CPU will access to SDRAM only when it is not needed to LTDC?

Maybe I have missed something?

Thanks!
    This topic has been closed for replies.

    1 reply

    Vladislav Yurov
    Associate III
    December 21, 2018

    Yes, you have missed Table 10, from the document ​https://www.st.com/resource/en/application_note/dm00287603.pdf