Skip to main content
Associate III
Mar 12, 2024 1:06 AM UTC
Question

STM32f429: reading 2.5V issue as soon as I connect the source to the ADC input

Hi 

I'm trying to read a 2.5V signal through internal adc as soon as I connect the signal to the gpio pin of stm there is shift(to positive side)in the signal and also generating the noise upon seeing through oscilloscope.

Also made ground connection.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Mar 12, 2024 1:18 AM UTC

What pin on what board?

Check the schematic to understand what might be on the pin

Perhaps use a opamp so as not to load the signal.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
harry123Author
Associate III
Mar 12, 2024 2:55 AM UTC

Pin PA4 

Using voltage divider to lower the voltage from 46V to 2.5V and giving the signal to Stm.