Question
STM32F429 NVIC Register Question
Posted on September 15, 2017 at 15:03
I want to know the NVIC Register
There is a description of GPIO and INTERRUPT in the Reference DataSheet, but there is no description of NVIC Register
Where can I find the details of the Register below?
typedef struct
{ __IOM uint32_t ISER[8U]; /*!< Offset: 0x000 (R/W) Interrupt Set Enable Register */ uint32_t RESERVED0[24U]; __IOM uint32_t ICER[8U]; /*!< Offset: 0x080 (R/W) Interrupt Clear Enable Register */ uint32_t RSERVED1[24U]; __IOM uint32_t ISPR[8U]; /*!< Offset: 0x100 (R/W) Interrupt Set Pending Register */ uint32_t RESERVED2[24U]; __IOM uint32_t ICPR[8U]; /*!< Offset: 0x180 (R/W) Interrupt Clear Pending Register */ uint32_t RESERVED3[24U]; __IOM uint32_t IABR[8U]; /*!< Offset: 0x200 (R/W) Interrupt Active bit Register */ uint32_t RESERVED4[56U]; __IOM uint8_t IP[240U]; /*!< Offset: 0x300 (R/W) Interrupt Priority Register (8Bit wide) */ uint32_t RESERVED5[644U]; __OM uint32_t STIR; /*!< Offset: 0xE00 ( /W) Software Trigger Interrupt Register */} NVIC_Type;