Skip to main content
zeus_zhn
Associate
Oct 21, 2014 7:55 AM UTC
Question

STM32F429 NAND conflict withSDRAM

Posted on October 21, 2014 at 09:55

I have a board based on the stm32f429. There is a 16M Bytes SDRAM (MT48LC16M8) and a 32M bytes NAND (NAND128W3A2B) connected to the FMC bus.

I used one area of the SDRAM as the LTCD buffer,such as:

 /* Start Address configuration : the LCD Frame buffer is defined on SDRAM */   

 LTDC_Layer_InitStruct.LTDC_CFBStartAdress = LCD_FRAME_BUFFER;

There is two strange problem:

[1] The nand write/read is always unstable, sometimes went wrong. After months of trying, I finally found that:

The nand operation is ok if I turn off the LTDC controller, namely not using the SDRAM as frame buffer. the command is:

 LTDC_Cmd(ENABLE);

[2] Even I turn off the LTDC controller, if I use the upper 8M bytes of sdram, the nand still generates write error.

To summarize:

The only working nand operation is to satisfy both:

a. Turn off the LCD controller;

b. configure the SDRAM as using 8M bytes only:

  FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_9b;

  FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b;

If I configure to use the whole 16M SDRAM like:

  FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_10b;

  FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b;

nand will go wrong.

I have researching this problem for months, can't find the answer, could anyone help me out. Even a hint maybe will help me find the solution.

Thank you very much!

If I only use the

    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    Oct 21, 2014 8:07 AM UTC
    Posted on October 21, 2014 at 10:07

    What Address bits does the NAND use to differentiate between the command/data interfaces? What timing/stability requirements does the NAND have wrt the data and address buses?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    zeus_zhn
    zeus_zhnAuthor
    Associate
    Oct 21, 2014 8:13 AM UTC
    Posted on October 21, 2014 at 10:13

    Both nand and sdram are 8 bits.

    For Nand, i mm using the wait feature, the configuration is:

        p.FMC_SetupTime     = 0x1;

        p.FMC_WaitSetupTime = 0x3;

        p.FMC_HoldSetupTime = 0x2;

        p.FMC_HiZSetupTime  = 0x1;

        FMC_NANDInitStructure.FMC_Bank = FMC_Bank2_NAND;

        FMC_NANDInitStructure.FMC_Waitfeature = FMC_Waitfeature_Enable;

        FMC_NANDInitStructure.FMC_MemoryDataWidth = FMC_NAND_MemoryDataWidth_8b;

        FMC_NANDInitStructure.FMC_ECC = FMC_ECC_Disable;

        FMC_NANDInitStructure.FMC_ECCPageSize = FMC_ECCPageSize_512Bytes;

        FMC_NANDInitStructure.FMC_TCLRSetupTime = 0x00;

        FMC_NANDInitStructure.FMC_TARSetupTime = 0x00;

    zeus_zhn
    zeus_zhnAuthor
    Associate
    Oct 21, 2014 12:38 PM UTC
    Posted on October 21, 2014 at 14:38

    I am not sure if I understanding this errota correctly, does this mean:

    SDRAM and NAND cannot be used at the same time in some chip production version?

    zeus_zhn
    zeus_zhnAuthor
    Associate
    Oct 22, 2014 7:46 AM UTC
    Posted on October 22, 2014 at 09:46

    Could anyone explain what does this workaround means regarding to the ''FMC dynamic and static bank switching''

    Description

    The dynamic and static banks cannot be accessed concurently.

    Workaround

    Do not use dynamic and static banks at the same time. The SDRAM device must be in self-refresh before switching to the static memory mapped on the Nor or NAND controller.

    Before switching from static memory to SDRAM, issue a normal command to wake-up the device from self-refres mode.

    Does my situation  means ''concurrently access'':

    reading/wring from NAND while the LTDC using SDRAM as framebuffer. The nand is using BANK 2, the SDRAM is using bank 5.

    waclawek.jan
    Super User
    Oct 22, 2014 8:38 AM UTC
    Posted on October 22, 2014 at 10:38

    Unfortunately, yes. The errata means, that to use NAND, you need to stop using SDRAM, and vice versa.

    JW

    zeus_zhn
    zeus_zhnAuthor
    Associate
    Oct 22, 2014 9:23 AM UTC
    Posted on October 22, 2014 at 11:23

    That doesn't make sense, because I can read/write nand directly to a SDRAM area if turn off the LTDC controller. Like:

    u8 pcDest[0x100000] __attribute__((at(0xc0200000)));

    uffs_read(fd, pcDest, header.ulFileSize);

    zeus_zhn
    zeus_zhnAuthor
    Associate
    Nov 18, 2014 2:06 PM UTC
    Posted on November 18, 2014 at 15:06

    So the only solution for me is to wait the version 3 chip?

    Tesla DeLorean
    Guru
    Nov 18, 2014 4:46 PM UTC
    Posted on November 18, 2014 at 17:46

    So the only solution for me is to wait the version 3 chip?

    This is a conversation you should be having with your local ST representatives and FAEs. They are much better placed to understand the problem, and any solutions, or timing of chip releases.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..