Skip to main content
chichkinei
Associate III
February 21, 2014
Question

STM32F429 LTDC driving SSD1289

  • February 21, 2014
  • 3 replies
  • 1341 views
Posted on February 21, 2014 at 02:40

Hi all. I'd like to incorporate this LCD into my project: http://www.mcu-turkey.com/wp-content/uploads/2013/12/3.2pi-ssd1289.pdf but I'm not sure it's possible to drive it with the LTDC. The display doesn't have VSYNC or HSYNC lines, it uses a simple 16-bit RGB565 interface along with WR(clock), CS, and RS. Before I start doing any in depth research and designing a circuit board, I'd like to know if it's possible to use the LTDC for a display like this. I'm also not sure what the LCD_DE line on the LTDC does.

    This topic has been closed for replies.

    3 replies

    chichkinei
    Associate III
    June 6, 2014
    Posted on June 06, 2014 at 09:30

    Ok, I've created a circuit board with the MCU and LCD and I've successfully bit-banged the protocol to test if it works. Now I need help with the LTDC code. Here is what I have so far

    #define LCD_WIDTH 240
    #define LCD_HEIGHT 320
    #define HFP 16//?????
    #define HSYNC 98
    #define HBP 48
    #define VFP 10
    #define VSYNC 2
    #define VBP 33
    #define ACTIVE_W (HSYNC + LCD_WIDTH + HBP - 1)
    #define ACTIVE_H (VSYNC + LCD_HEIGHT + VBP - 1)
    #define TOTAL_WIDTH (HSYNC + HBP + LCD_WIDTH + HFP - 1)
    #define TOTAL_HEIGHT (VSYNC + VBP + LCD_HEIGHT + VFP - 1)
    /* Pixel width in bytes */
    #define PIXELWIDTH 2
    static
    const
    GPIO_TypeDef * 
    const
    GPIOInitTable[] = {
    GPIOF, GPIOG, GPIOG, GPIOG, GPIOG, GPIOH, GPIOH,
    GPIOH, GPIOH, GPIOH, GPIOH, GPIOH, GPIOI, GPIOI,
    GPIOI, GPIOI, GPIOI, GPIOI,
    0};
    static
    uint8_t 
    const
    PINInitTable[] = {
    10, 6, 7, 11, 12, 9, 10,
    11, 12, 13, 14, 15, 0, 1,
    2, 5, 6, 7,
    0};
    static
    uint8_t 
    const
    AFInitTable[] = {
    14, 14, 14, 14, 14, 14, 14,
    14, 14, 14, 14, 14, 14, 14,
    14, 14, 14, 14,
    0};
    int
    main(
    void
    )
    {
     //excluded code which fills SDRAM with image data 
    LCD_Init();
    //bit-bang init
    paint(GREEN);
    //still bit-banged
    CLR_CS;
    set_Cursor(0,0,239,320);
    SET_RS;
    //prepare lcd to accept data. At this point all the LTDC needs to do is put data on the lines and pulse /WR 76800 times
    TFTLCD_Init();
    while
    (1){}
    }
    void
    gpio_conf(GPIO_TypeDef * GPIO, uint8_t pin, uint8_t mode, uint8_t type, uint8_t speed, uint8_t pullup, uint8_t af)
    {
    GPIO->MODER = (GPIO->MODER & MASK2BIT(pin)) | (mode << (pin * 2));
    GPIO->OTYPER = (GPIO->OTYPER & MASK1BIT(pin)) | (type << pin);
    GPIO->OSPEEDR = (GPIO->OSPEEDR & MASK2BIT(pin)) | (speed << (pin * 2));
    GPIO->PUPDR = (GPIO->PUPDR & MASK2BIT(pin)) | (pullup << (pin * 2));
    if
    (pin > 7)
    {
    GPIO->AFR[1] = (GPIO->AFR[1] & AFMASKH(pin)) | (af << ((pin - 8) * 4));
    }
    else
    {
    GPIO->AFR[0] = (GPIO->AFR[0] & AFMASKL(pin)) | (af << ((pin) * 4));
    }
    }
    void
    TFTLCD_Init(
    void
    )
    {
    uint8_t i = 0;
    /* GPIO pin configuration */
    while
    (GPIOInitTable[i] != 0){
    gpio_conf(GPIOInitTable[i], PINInitTable[i], MODE_AF, TYPE_PUSHPULL, SPEED_100MHz, PULLUP_NONE, AFInitTable[i]);
    i++;
    }
    /* PLL */
    RCC->PLLSAICFGR = (49 << 6) | (7 << 24) | (7 << 28);
    /* Enable SAI PLL */
    RCC->CR |= RCC_CR_PLLSAION;
    /* wait for SAI PLL ready */
    while
    ((RCC->CR & RCC_CR_PLLSAIRDY) == 0);
    /* enable clock for LTDC */
    RCC->APB2ENR |= RCC_APB2ENR_LTDCEN;
    /* Synchronization Size Configuration */
    LTDC->SSCR = ((HSYNC - 1) << 16) | (VSYNC - 1);
    /* Back Porch Configuration */
    LTDC->BPCR = ((HBP - 1) << 16) | (VBP - 1);
    /* Active Width Configuration */
    LTDC->AWCR = (ACTIVE_W << 16) | (ACTIVE_H);
    /* Total Width Configuration */
    LTDC->TWCR = (TOTAL_WIDTH << 16) | (TOTAL_HEIGHT);
    /* Window Horizontal Position Configuration */
    LTDC_Layer1->WHPCR = HBP | ((HBP + LCD_WIDTH - 1) << 16);
    /* Window Vertical Position Configuration */
    LTDC_Layer1->WVPCR = VBP | ((VBP + LCD_HEIGHT - 1) << 16);
    /* Pixel Format Configuration */
    LTDC_Layer1->PFCR = 2;
    /* Color Frame Buffer Address */
    LTDC_Layer1->CFBAR = SDRAM_BANK_ADDR;
    /* Color Frame Buffer Length */
    LTDC_Layer1->CFBLR = ((LCD_WIDTH * PIXELWIDTH) << 16) | ((LCD_WIDTH * PIXELWIDTH) + 3);
    /* Enable Layer */
    LTDC_Layer1->CR = LTDC_LxCR_LEN;
    /* Immediate Reload */
    LTDC->SRCR = LTDC_SRCR_IMR;
    LTDC->GCR = LTDC_GCR_PCPOL; 
    // /WR is active low
    /* Enable LTDC */
    LTDC->GCR |= LTDC_GCR_LTDCEN;
    }

    As this LCD doesn't take HSYNC and VSYNC signals, it has no specs for VFP, VBP, HFP etc. so I don't know what to set these to. Currently I just get a black screen after the LTCD init function instead of the image data that's in the SDRAM and the pixel clock (/WR) is pulsing continuously, whereas I need it to stop every 76800 pulses so I can reset the cursor to (0, 0).
    chichkinei
    Associate III
    June 6, 2014
    Posted on June 06, 2014 at 09:31

    double (surprisingly not quadruple) post...

    Montassar BEN ROMDHANE_O
    Visitor II
    January 15, 2015
    Posted on January 15, 2015 at 12:03

    Hi,

    The SSD1289 LCD is supported by STemWin since 5.18 version. You have just need to configure the LCDConf file (by adding the basic write/read operation) and call the right controller in LCD_X_Config (for SSDD1289: GUIDRV_FLEXCOLOR_F66702)

    Keep us informed about your finding.

    Regards,

    Heisenberg.