Skip to main content
shiwei luan
Visitor II
March 27, 2018
Question

STM32F429: GPIO logic level during power on

  • March 27, 2018
  • 1 reply
  • 651 views
Posted on March 27, 2018 at 03:10

What is the logic level of GPIO pins of STM32F429 during powering on?

I am using several GPIO pins as enable pins to enable downstream devices. These GPIOs must be 'LOW' during power on until the firmware actively enables them.

I tried to find information from datasheet, but this information is not specified. My question is: when STM32F429 is being powered on and before the firmware takes care of GPIO configurations, what is the status of GPIO, HIGH, LOW or HIGH Z?

Thank you.

    This topic has been closed for replies.

    1 reply

    waclawek.jan
    Super User
    March 27, 2018
    Posted on March 27, 2018 at 09:46

    Unless it's one of the JTAG/SWI pins, and unless you enable bootloader, they are floating - see RM0090 rev.15, 8.3.1  General-purpose I/O (GPIO).

    Use an external pulldown if you need a defined logic level during powerup.

    JW