Question
STM32F429 FPU hard enabled, still seeing float functions in assembly
-mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard I am building my project with above options and enabling the FPU unit
void System::enableFPU()
{
SETVALUE(FPUB->CPACR , ((3UL << 10*2) | /* set CP10 Full Access */
(3UL << 11*2) )); /* set CP11 Full Access */
}What is interesting is that in the dump output I can still see
1> 134218232 00000352 T __aeabi_fadd
1> 134218228 00000356 T __aeabi_fsubI was expecting that instead of fadd,fsub library FPU instructions would be used.
Is this normal behaviour or am I missing something in the configuration?
when float-abi=soft is set I get some more functions. So it seems that fmul and fdiv are supported by float-abi but fadd and fsub are not ?
1> 134219120 00000310 T __aeabi_fdiv
1> 134219120 00000310 T __divsf3
1> 134218232 00000352 T __aeabi_fadd
1> 134218228 00000356 T __aeabi_fsub
1> 134218228 00000356 T __subsf3
1> 134218760 00000360 T __aeabi_fmul