Skip to main content
alireza_roozitalab
Associate III
January 23, 2016
Question

stm32f429 etm trace

  • January 23, 2016
  • 2 replies
  • 692 views
Posted on January 23, 2016 at 14:24

hello i want to use 4pin etm trace (ukink pro )on stm32f429

and i have this problem:

if  core clock > 100 mhz i cant use etm trace

and if core clock<140 mhz i cant use ltdc

is there any true configs for use etm trace on 180 mhz ?

or how can i use ltdc  in core clock <140 mhz?

best regards
    This topic has been closed for replies.

    2 replies

    re.wolff9
    Senior
    January 24, 2016
    Posted on January 24, 2016 at 10:09

    I had to look up what LTDC is. It's a TFT interface. 

    In my experience LCD will work at lower clocks than nominal. If something claims it won't work below 140MHz, you might ''cheat'' and e.g. tell everything that you have a 16MHz external crystal while in fact you have a 8MHz one. Now the CPU will run at 90MHz, the LCD will refresh at 30Hz instead of 60Hz, but  maybe the ETM might work.... 

    alireza_roozitalab
    Associate III
    January 24, 2016
    Posted on January 24, 2016 at 12:45

    first of all thanks for your replay

    yes  I use tft lcd 8 inch (480*800 pixel) in RGB888 mode

    and my sdram is k4s561632c

    board crystal is 8mhz

    i self designed board with stm32f429IIT

    and have not any problem with ltdc peripherals(tft lcd) if core clock>140mhz .

    i check sdram by writing and reading value and check them in core clock lower than 140 mhz and i seen that every ting work correctly

    and i use const picture in flash of micro to show on lcd  (without using sdram) and i seen that it work true on core clock <140mhz !!!!!!!

     but i cant used sdram and ltdc with each other in core clock <140 mhz  , the lcd show is unclear

    best regards