Skip to main content
Associate II
January 23, 2025
Question

Stm32f429 disco integration with finger print sensor using spi

Hello..

I am using STM32F429 Disco Board in which I am trying to interface finger print sensor NB65210 of next biometric using spi and I need to read the finger print data I have a example code in which it is reading properly but it is not reading when I configured for myself l, I have selected proper clock, spi pins, Chip select nreset, nawake, the library which ever they have given I have not modified NBdeviceInitializationA  it is getting nbok but after that stocking and giving error code for all library function what will the issue can anyone suggest the solution...

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
January 24, 2025

@Abhishek_nr wrote:

I have a example code in which it is reading properly but it is not reading when I configured for myself l


So carefully compare & contrast your implementation against the working one.

Have you checked the interface lines with an oscilloscope and/or logic analyser to see what's actually happening on the wires?

 


@Abhishek_nr wrote:

finger print sensor NB65210 


Please post a link to its documentation.

Please post your schematic.

See: How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.