Skip to main content
ASSAAD.ASSAAD
Associate III
December 26, 2017
Question

STM32f429 ( 144) , port PA0 input problem

  • December 26, 2017
  • 1 reply
  • 551 views
Posted on December 26, 2017 at 09:00

Hello 

we are using STM32f429 ( 144)  ,we use port PA0 as input without interrupt ; PA0 has an external pull up resistor ; 

we use the it on 168Mhz  with external crystal  8Mhz , 

but we noticed that we cant configure this pin input and the voltage go down to 1.2V ! on PA0  ; this happen while configuring the clock of the system . 

static void SystemClock_Config(void)

{

RCC_ClkInitTypeDef RCC_ClkInitStruct;

RCC_OscInitTypeDef RCC_OscInitStruct;

/* Enable Power Control clock */

__HAL_RCC_PWR_CLK_ENABLE();

/* The voltage scaling allows optimizing the power consumption when the device is

clocked below the maximum system frequency, to update the voltage scaling value

regarding system frequency refer to product datasheet. */

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

//

/* Enable HSE Oscillator and activate PLL with HSE as source */

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 8;

RCC_OscInitStruct.PLL.PLLN = 336;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

RCC_OscInitStruct.PLL.PLLQ = 7;

HAL_RCC_OscConfig (&RCC_OscInitStruct);

/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2

clocks dividers */

RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);

}

Any help here please  ? 

Thank you in advanced 

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    December 26, 2017
    Posted on December 26, 2017 at 18:07

    You're going to have to look critically at what you have the pin attached to in your design. Disconnect other circuitry and confirm pin behaves as expected then. If it does you know it is about what you are attempting to drive the pin with.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..