Skip to main content
NPuts.1
Visitor II
October 10, 2022
Solved

STM32F427ZIT6 Maximum voltage on PA0 when used as analog (ADC) input

From the datasheet PA0 is listed as a 5V tolerant IO (FT type).

Does this maximum of 5V still hold if the pin is mapped to the ADC input? If not, what is the maximum reading for this case?

This topic has been closed for replies.
Danish1
Danish1Best answer
Lead III
October 10, 2022

According to the Reference Manual section 8.3.12 "Analog configuration"

In the analog configuration, the I/O pins cannot be 5 Volt tolerant.

In this case I would expect the maximum to be Vdd. (Strictly speaking Vdd + 0.3 V).

Hope this helps,

Danish

2 replies

Danish1
Danish1Best answer
Lead III
October 10, 2022

According to the Reference Manual section 8.3.12 "Analog configuration"

In the analog configuration, the I/O pins cannot be 5 Volt tolerant.

In this case I would expect the maximum to be Vdd. (Strictly speaking Vdd + 0.3 V).

Hope this helps,

Danish

waclawek.jan
Super User
October 10, 2022

There's also footnote (5) to the pin definitions table, saying

FT = 5 V tolerant except when in analog mode or oscillator mode (for PC14, PC15, PH0 and PH1).

> In this case I would expect the maximum to be Vdd. (Strictly speaking Vdd + 0.3 V).

Strictly speaking VDDA+0.3V, but in 'F4 there's also a requirement for VDDA=VDD.

JW