Question
STM32f427 SAI Clock Problems
Posted on October 30, 2015 at 14:56
Hi
I am struggling to get the External Audio Clock Input (PC9 12.288MHZ) to be output by the SAI Master clock pin PF7. I have used STM32Cube to set it up and it all looks ok, but I can not get any output on the SAI Master Clock even if i try and use the internal PLL clock. I am trying to communicate with a SSM2604 codec, I can see the clock is correct on the SAI_SCK_B (PF8) and I get a pulse on SA1_FS_B but SA1_MCLK is Dead I am using SAI_B in master mode with Master Clock Out. Any Help, examples etc would be gratefully received Thanks John