Question
STM32F427 Inverted DAC output
Posted on July 07, 2015 at 20:13
I've seen at least two other threads with an inverted DAC concern being present, wondering if anyone has more information o the issue? I have 3 identical boards in house populated with the F4, one of which has an inverted DAC output.
I'm not finding any errata on this, only seeing others experiencing a similar issue.All three boards are running identical code. All boards seem to work properly in GPIO mode. My sample size on this issue is small, but if this is a possible concern to any magnitude I would like to identify it before it is too late in the development process. Any input that may be out there would be very helpful. #dac-inverted-stm32f4