Skip to main content
Yuktheshwar Bhat
Associate II
June 6, 2018
Question

stm32f417 cryptography

  • June 6, 2018
  • 8 replies
  • 2315 views
Posted on June 06, 2018 at 07:43

Hi am a beginner in the stm32f417 micro controller programming.Can anybody help me regarding how to implement cryptography in stm32f417vg micro controller.

    This topic has been closed for replies.

    8 replies

    Tesla DeLorean
    Guru
    June 6, 2018
    Posted on June 06, 2018 at 13:46

    ST has a Crypto library available.

    http://www.st.com/en/embedded-software/stm32-cryp-lib.html

     

    http://www.st.com/en/embedded-software/x-cube-cryptolib.html

     

    Both the SPL and HAL software trees have example code

    STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Project\STM32F4xx_StdPeriph_Examples\CRYP\CRYP_AES_CCM

    STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Examples\CRYP\CRYP_AES_DMA

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Yuktheshwar Bhat
    Associate II
    June 6, 2018
    Posted on June 06, 2018 at 16:07

    thank you...

    Nesrine M_O
    Associate
    June 7, 2018
    Posted on June 07, 2018 at 11:21

    https://community.st.com/0D50X00009bMM5DSAW

     
    Yuktheshwar Bhat
    Associate II
    June 12, 2018
    Posted on June 12, 2018 at 12:07

    Hi all..

    In stm32f4XX,  whether CRYP periferal have any dependencies on RTOS

    Tesla DeLorean
    Guru
    June 12, 2018
    Posted on June 12, 2018 at 15:44

    Well you'd need to serialize access to the hardware, I'd assume.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Yuktheshwar Bhat
    Associate II
    June 13, 2018
    Posted on June 13, 2018 at 11:42

    #include 'main.h'

    #include 'stm32f4xx_hal.h'

    CRYP_HandleTypeDef hcryp;

    void SystemClock_Config(void);

    static void MX_GPIO_Init(void);

    static void MX_CRYP_Init(void);

    int main(void)

    {

        uint8_t Plain_Data[1] = {10};

        uint8_t AEC_ECB_Encrypted_Data[1] = {0};

        uint8_t AEC_ECB_Decrypted_Data[1] = {0};

        HAL_Init();

        SystemClock_Config();

        MX_GPIO_Init();

        MX_CRYP_Init();

    while (1)

        {

            // encrypt the data

            if(HAL_CRYP_AESECB_Encrypt(&hcryp,Plain_Data,sizeof(Plain_Data),AEC_ECB_Encrypted_Data,1000) != HAL_OK)

            HAL_NVIC_SystemReset();

            // decrypt the encrypted data5

            if(HAL_CRYP_AESECB_Decrypt(&hcryp,AEC_ECB_Encrypted_Data,sizeof(AEC_ECB_Encrypted_Data),AEC_ECB_Decrypted_Data,10) != HAL_OK)

               HAL_NVIC_SystemReset();

        }

    }

    am using the above code to encrypt and decrypt the data but when i do decryption of encrypted data am not getting original data.

    Tesla DeLorean
    Guru
    June 13, 2018
    Posted on June 13, 2018 at 15:32

    I don't think working with one byte buffers is how this functions.

    ST has AES examples, work with those.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Yuktheshwar Bhat
    Associate II
    June 14, 2018
    Posted on June 14, 2018 at 08:51

    yes,I tried with the example given by the ST but the encrypted data is not matching with expected result.