Skip to main content
Shush1908
Associate II
May 2, 2023
Question

STM32F412 STOP mode HAL_RTC_GetTime return time before sleep

  • May 2, 2023
  • 1 reply
  • 897 views

Hi,

I work with STM32F412/STM32F413 processor. I have also external LSE.

I have the next problem related to STOP mode and RTC.

There are some scenarios we want the processor to go to sleep for x hours.

The processor goes to sleep for 5 seconds, doing some job and return to sleep for 5 seconds and so on in infinite loop till it is broke by interrupt or if time elapsed( the x hours ).

The problem is that sometimes during the sleep phase - The RTC read after HAL_PWR_EnterSTOPMode is the same as before(sleepTime =0) even if in fact the processor sleeps for 5 seconds(We checked it by led and by debug code). This causes the total sleep time to increase and awakening delayed after several hours!!!!

I thought that maybe because the RTC is not ready between HAL_PWR_EnterSTOPMode and the RTC read, so I added a delay after HAL_PWR_EnterSTOPMode line and also add after the delay a piece of code that if sleepTime is 0 -> reading again the RTC. It seems that it solved the problem, but this is not solution I like and it looks bad. I prefer to a solution to read a register or a variable and by that to know that the RTC is ready to be read.

The next is a sample of the relevant code(without my "solution"):

HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 5 , RTC_WAKEUPCLOCK_CK_SPRE_16BITS) ;

RTC_TimeTypeDef sTimeBefore , sTimeAfter ;

RTC_DateTypeDef sDateBefore , sDateAfter ;

int sleepTime = 0 ;

int totalSleepTime = 0 ;

.

.

.

.

while( sleep )

{

 ReadRTC( &sTimeBefore , &sDateBefore ) ; // This function call to HAL_RTC_GetTime function and

// after that to HAL_RTC_GetDate function

 HAL_PWR_EnterSTOPMode( PWR_LOWPOWERREGULATOR_ON , PWR_STOPENTRY_WFE ) ;

 ReadRTC( &sTimeAfter , &sDateAfter ) ;

 sleepTime = CalculateSleepTime( sTimeBefore , sDateBefore , sTimeAfter , sDateAfter ) ;

 totalSleepTime += sleepTime ;

 if ( totalSleepTime > x )

  sleep = 0 ;

}

.

.

.

.

Please any assistance.

Shai

This topic has been closed for replies.

1 reply

Shush1908
Shush1908Author
Associate II
May 2, 2023

h