Skip to main content
Associate
August 18, 2024
Solved

STM32F411CEUx USB Serial Port Issue

I am having trouble configure the USB-C port for serial output. The board I got is a "BlackPill" and I have went to try some example code for USART2 and USART6, however, upon a reset, I still do not have a COM port appear. Any advice?

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
August 18, 2024

Where you expecting to see a com port when running a UART?

If you want to get something on USB connection, like a VCP, you have to run something that doing the handling on the USB bus: so use a serial to USB adapter, connected to the UART you want to use, or set in Cube the USB -> device -> virtual com Port, to let it include all the libraries and USB stack to do the action, that's needed for a USB VCP to work.

Read examples or here in forum how to use it then.

If you feel a post has answered your question, please click on " Best Answer ".

1 reply

AScha.3
AScha.3Best answer
Super User
August 18, 2024

Where you expecting to see a com port when running a UART?

If you want to get something on USB connection, like a VCP, you have to run something that doing the handling on the USB bus: so use a serial to USB adapter, connected to the UART you want to use, or set in Cube the USB -> device -> virtual com Port, to let it include all the libraries and USB stack to do the action, that's needed for a USB VCP to work.

Read examples or here in forum how to use it then.

If you feel a post has answered your question, please click on " Best Answer ".