Skip to main content
Ludovic Durand-Texte
Associate II
May 25, 2018
Question

STM32F411 VCP USB OTG Problem (don't start)

  • May 25, 2018
  • 2 replies
  • 858 views
Posted on May 25, 2018 at 02:23

Hi,

I am using the STM32_USB-Host-Device_Lib_V2.2.0 and more specifically the STM32_USB_OTG_Driver and STM32_USB_Device_Library.

I have made running the VCP connection with an STMF405 with no problem.

Now using an STMF411, the connection does not establish : The Usb packet 'device connected' on the other end does not contains the VID nor the PID.

Tracing the interruptions in the usb_dcd_int.c, I noticed that the process does not follow the same sequence:

- With the F405 the sequence is usbreset .. enumdone .. rxstsqlvl .. outepintr where the description is sent. (in the middle of each interruption, there is several sofintr that I omit here).

- With the F411 and the same code, the sequence loops as [usbreset .. enumdone ..] 4 times and ends with a usbsuspend. (without any sofintr in between)

I have checked the frequency on the line with the oscilloscope, it is ok

I have compared the values of each variable/register between the F405 and F411 during the usbreset and enumdone, I have exactly the same values.

I do not know the protocol but what I see is that interruptions that should raise after usbreset and enumdone does not. So the USBD_VID and USBD_PID are never sent.

Does someone have an idea of where I am wrong and/or what to check or trace?

Regards,

Ludovic

#stm32f405-stm32f411-stm32_usb_otg_driver-stm32_usb_devi
This topic has been closed for replies.

2 replies

Ludovic Durand-Texte
Associate II
May 25, 2018
Posted on May 25, 2018 at 15:39

Correction:

- With the F411 and the same code, the sequence loops as [usbreset .. enumdone ..

sofintr ... sofintr...

] 4 times and ends with a usbsuspend.
Ludovic Durand-Texte
Associate II
May 26, 2018
Posted on May 27, 2018 at 01:47

Hi,

Problem solved.

The PLL configuration given with the library was wrong on PLL_N. The PLL_x values were not ok to give the needed 48KHz clock.

Always check in detail the PLL and dividers first