Skip to main content
nickcupery
Associate II
March 19, 2016
Question

STM32F410 Elf Loader Problem

  • March 19, 2016
  • 23 replies
  • 4966 views
Posted on March 19, 2016 at 15:23

  I have a brand-new project (with brand-new circuit board) based

on the STM32F410CBT6 chip.  This chip, which I think is relatively

new, supposedly has 128KB of FLASH and 32KB of SRAM.  However, the

default linker script provided by STM incorrectly says the FLASH

is 64KB.  So, I corrected the linker script and I will (try to)

attach a copy.

  Like all of my STM projects, this is a VisualGDB project (and

VisualGDB is the best thing since sliced bread).  Thus, I first

noticed my STM32F410 problem when I tried to load/debug the new

program with VisualGDB.  VisualGDB claims the stack address

0x20007FFC is not writable, yet the data sheet (and the linker

script) say that address is perfectly legal.  When I tried a

much lower value for _estack, I got the same failure but with

the new supposedly illegal address correctly indicated in the

error message.

  So I then tried to load my new program with STM's ST-Link

Utility program.  No joy!  ST-Link Utility connects to the

device and correctly identifies it as an STM32F410xx Rev A,

but when I try to ''erase chip'' I get a MessageBox saying that

''the elf loader is bigger than the RAM size''.  When I explicitly

tell ST-Link Utility to examine SRAM memory addresses, it does

successfully access the addresses from 0x20000000 to 0x20007FFC,

and then fails at 0x20008000 as expected.  Hmmm.  So, how big

is this ''elf loader'' anyway?  Does anyone know?  I don't really

know anything about elf loaders, but I've written a few ''loaders''

in my day and they are all just a coupla hundred bytes of tightly

coded assembly language -- certainly nothing approaching 32KB!

  Ideas?  Note that I've run this problem by the VisualGDB folks

(who provide TOP QUALITY tech support), and they haven't seen

this one before.

  Maybe I've purchased a load of Rev A chips that don't work?  

I'm not fond of that answer. :)

- eNick

#tl
    This topic has been closed for replies.

    23 replies

    Radosław
    Associate II
    April 5, 2016
    Posted on April 05, 2016 at 18:41

    >>Indeed, but the processor still expects you to set a valid stack address, and when things fault or interrupt, it is going to use that.

    Any function is enough to use stack

    Tesla DeLorean
    Guru
    April 5, 2016
    Posted on April 05, 2016 at 19:03

    Any function is enough to use stack

    Single depth call does not.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    nickcupery
    Associate II
    April 6, 2016
    Posted on April 06, 2016 at 13:19

    >the processor still expects you to set a valid stack address,

    >and when things fault or interrupt, it is going to use that.

      My test program has a pefectly valid stack address at the

    beginning of the interrupt vector table, right where it belongs.

    I have an LED that gets lit up by the default interrupt handler

    if ANY interrupt or fault occurs.  None occurs.

    >You can write things that don't use RAM, but it is highly atypical

      Atypical and then some!  This is a test program, Clive. :)

    It is carefully contrived to NOT use any SRAM.  No stack.  No

    functions.  Code only, and little of it, in flash.

      If I could figure out how to attach code and screen snapshots

    using this demented forum software, I would do so and also award

    myself a PhD in foreign languages.  

      Please remember that I have moved beyond asking ''why doesn't

    my test program work'', to asking ''why doesn't ST-Link Utility

    correctly load my program''.  The problem doesn't really have

    anything to do with my program itself.  When I *FORCE* STLU to

    load my program (by terminating/restarting STLU, as stated in

    my previous message) my program works just fine.

      I don't really expect to find that there is some fundamental

    ''show stopper'' of a problem with the F410.  Rather, I expect

    that it will turn out that there is ''something about the chip''

    that requires a modification to VisualGDB/OpenOCD and also to

    the ST-Link Utility.  (BTW, according to STM Support, the latest

    version of STLU exists BECAUSE of a required modification for

    the F410.  I think STLU requires an ADDITIONAL modification,

    which will need to be propagated to VisualGDB/OpenOCD.)

      Apparently, I am the ONLY guy on Earth who has tried to use

    the F410.  The only one who is willing to talk about it, anyway.

    There are probably a few who have discovered the required

    workaround and just kept quiet about it.

      I should mention that I am very pleased with the STM Tech

    Support folks.  They respond to my problem report ''tickets''

    quickly and in reasonable depth.  They are looking at this

    problem right now.  The only thing about STM tech support

    that bothers me is that THEIR (apparently separate) forum

    software is FAR MORE DEMENTED than what we are dealing with

    here.  I have very little confidence that they are seeing

    all the stuff I send them.  All efforts to have them simply

    call me on the phone have so far failed.  Still, compared

    to Atmel, ST Micro is Tech Support Heaven.

     - eNick