Skip to main content
Associate II
Jun 5, 2024 6:33 AM UTC
Solved

STM32F407ZGT6 +LAN8720+FREERTOS+LWIP+HTTPD《LwIP_HTTP_Server_Raw》

@
STM32Cube_FW_F4_V1.28.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw
I use this Demo,replace phy with Lan8742 sucessfully,then I ping this board ip address sucessfully too,but when I open webpage by browser,the network is down,cannot ping ,how to solve this problem。

with
STM32Cube_FW_F4_V1.26.2\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw
this version can work whole time.Compare two versions,different files are HAL Drivers  and ethernetif.c.so
how to solve this problem,thanks for your help!

 

This topic has been closed for replies.
STeaBest answer
ST Employee
Jul 4, 2024 12:57 PM UTC

Hello @ZainFan ,

by costume board I mean is this a Custom PCB that you are using this is not a board provided by ST so you need to make sure that you are rooting the correct pins to the PHY interface are the same (check pinouts in the Ethernetif.c to look for changes as the example you put don't use the same PHY. also make sure you are using the correct lan8720.c file.
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

ST Employee
Jun 13, 2024 3:12 PM UTC

Hello @ZainFan ,

thank you for sharing this with us.

could you please give us some details to help us reproduce you issue?

about the Hardware you are using?

is the STM32F407ZGT6 +LAN8720 a custom board? 

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ZainFanAuthor
Associate II
Jun 17, 2024 9:05 AM UTC

sorry ,idont know what is  a custom board?  I buy it online。i can support a link to my code。

https://github.com/zainFan/STM32.git

thanks for your help ,you can find me with my email 1019472847@qq.com

STeaBest answer
ST Employee
Jul 4, 2024 12:57 PM UTC

Hello @ZainFan ,

by costume board I mean is this a Custom PCB that you are using this is not a board provided by ST so you need to make sure that you are rooting the correct pins to the PHY interface are the same (check pinouts in the Ethernetif.c to look for changes as the example you put don't use the same PHY. also make sure you are using the correct lan8720.c file.
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
Aug 2, 2024 11:19 AM UTC

Hello @ZainFan,

Did you manage to solve this issue? is there any updates?
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
Mar 18, 2025 6:26 AM UTC

Hello, @STea 

I have the same problem. The development board is also STM32F407ZGT6 + LAN8720. Using the httpd.c file to configure the webServer, I can ping the network, but after entering the IP configured for the PHY locally, the webpage cannot return resources, and afterwards I can no longer ping.

Regards