Skip to main content
Bruno Brentegani
Associate
Apr 20, 2018 12:47 PM UTC
Question

STM32F407VGXT DIscovery GPIO state at start_up

Posted on April 20, 2018 at 14:47

Hi all,

I'm using stm32f4 discovery with HAL drivers to realize a Synchronous BOOST DCDC.

When the system is turn on, the gpio PE8 and PE9 configured as PWM pins of TIM1,(in particular PWMOUT_CH1 & PWMOUT_CH1N) goes in SET state and for a  few milliseconds keep the mos of the converter in ON state causing a little initial short circuit.

At startup PE8 and PE9 are in high impedance state?

If so,can i avoid this issue with a 100k pull down resistors?

There are software solutions to this problem?

Best regards

Bruno

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Apr 20, 2018 1:06 PM UTC
    Posted on April 20, 2018 at 15:06

    >>There are software solutions to this problem?

    Not on the F4 series, best to define default high-low states with external pull up/down resistors. Placing code to program the GPIO in the Reset_Handler can reduce the time they are in undesirable states as subsequent code will spin up clocks and PLLs.

    I think one of the L4 or newer families provides a means of defining pin states at startup

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Bruno Brentegani
    Associate
    Apr 20, 2018 3:09 PM UTC
    Posted on April 20, 2018 at 15:09

    Thanks Clive one