Associate III
October 13, 2012
Question
stm32f407vgt6
- 18 replies
- 3444 views
Posted on October 13, 2012 at 16:43
hi,
i have stm32 discovery board(stm32f407vgt6) and a new stm32f407vgt6 ic.i want to program the new stm32f407vgt6 ic.so i change the hardware settings in my discovery board.In discovery board contains STM32F103C8T6 and stm32f407vgt6.STM32F103C8T6 connected to stm32f407vgt6 through:1.TCK/SWCLK-PA142.TMS/SWDIO-PA133.T_NRST-NRST4.T_SWO-PB35.MCOBYso i break the setting of discovery between STM32F103C8T6 and stm32f407vgt6.now i set the new setting between STM32F103C8T6 of discovery and my new stm32f407vgt6 according to the old setting of the discovery.now i get the 50 percent positive result.That means i can connect the device( new stm32f407vgt6) via stm32 st-link utility software.it reads device and device id of the new stm32f407vgt6.but it gives warning .i attached the png file about warning.please find it.i cannot read the memory.give any suggestion in my connection. #wait-for-you--clive1-!-!-! #wait-for-you #wait-for-you--clive1-!-!-!