Associate II
March 17, 2016
Question
STM32F407VGT-DISCOVERY Cirrus 43L22 year 2016 HAL library incomplete?
- March 17, 2016
- 2 replies
- 1647 views
Posted on March 18, 2016 at 00:59Hi Everyone,Simple question:Is the STM32F407VGT-DISCOVERY Cirrus 43L22 HAL library released incomplete?In the HAL library source and header files cs44l22.h and cs43l22.c I find the following obviously incomplete code!Example:/** * @brief Sets new frequency. * @param DeviceAddr: Device address on communication Bus. * @param AudioFreq: Audio frequency used to play the audio stream. * @retval 0 if correct communication, else wrong communication */uint32_t cs43l22_SetFrequency(uint16_t DeviceAddr, uint32_t AudioFreq){ return 0;}Nothing is obviously happening in the code above so why is it there?Another one here:/** * @brief Start the audio Codec play feature. * @note For this codec no Play options are required. * @param DeviceAddr: Device address on communication Bus. * @retval 0 if correct communication, else wrong communication */uint32_t cs43l22_Play(uint16_t DeviceAddr, uint16_t* pBuffer, uint16_t Size){ uint32_t counter = 0; if(Is_cs43l22_Stop == 1) { /* Enable the digital soft ramp */ counter += CODEC_IO_Write(DeviceAddr, CS43L22_REG_MISC_CTL, 0x06); /* Enable Output device */ counter += cs43l22_SetMute(DeviceAddr, AUDIO_MUTE_OFF); /* Power on the Codec */ counter += CODEC_IO_Write(DeviceAddr, CS43L22_REG_POWER_CTL1, 0x9E); Is_cs43l22_Stop = 0; } /* Return communication control value */ return counter; }In the above code the most important values pBuffer and Size are not used. How comes?And a last one here:/** @defgroup CS43L22_Function_Prototypes * @{ */static uint8_t CODEC_IO_Write(uint8_t Addr, uint8_t Reg, uint8_t Value);/** * @} */ If anyone can tell me what the above function is doing I'd be most happy.Thx for sharing the state of affairs.Greets,Ben #cs44l22-stm32f4-stm32f4discovery