First of all you need to establish a complete CAN bus with at least two CAN nodes. Then, in your case, the first node contains STM32F407 MCU with a CAN transceiver + a terminating resistor of 120 ohm and the second node a CAN/USB adapter on which you need to enable an internal 120ohm terminating resistor.
This is a minimal CAN bus structure:
https://community.st.com/t5/stm32-mcus/stm32-fdcan-running-at-8-mb-s-on-nucleo-boards/ta-p/730281?lightbox-message-images-730281=90488iD4EA082CEF3B11D9
I cannot give a recommendation for an USB-to-CAN adapter. But I can give an example: https://www.waveshare.com/usb-can-a.htm
But this is not a recommendation it's up to you to decide as this is not an ST product.
Meanwhile, from the microcontroller side, you need to add a transceiver for example what was used on several ST boards: SN65HVD230.
CAN communication example is provided here.
If you are not familiar with the CAN bus you need to study it before going ahead with using as communication medium.
Hope that helps.
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.