stm32f407vet6 MCU general questions
Hey everyone, I'm new to these microcontrollers and new to these MCUs in general, and had a few questions... First off, i have some experience using Arduinos, so I'm somewhat familiar with the functionality and programming involved, and I've done all the research I can as far as finding the compatible software for programming, and looking more into the arm assembly language involved (in case I need it alongside c), but I wanted to ask more about the capabilities of the board, and whether or not I can do certain things.
The board Ive ordered has a built in SD card reader and claims to have pins supporting an LCD screen, wireless, etc... So I was wondering if it may or may not be possible to run a light version of Linux (with a GUI) off of it, maybe using a Bluetooth keyboard and mouse. The only operating system I've found is the rtos, which definitely seems appealing for its own ease of use and purposes, but I was wondering if these boards were even capable of running anything with a GUI, if optimally configured (or if any such thing may already exist). Thanks!
*As a side note, I'm not necessarily asking if it's already been done, I would just as well be interested in doing it myself, just wondering if the capabilities may or may not potentially be there. Thanks!