STM32F407IGT6 ADC Input Range
Hello,
Am using STM32F407IGT6 in my design. I power the VDD, VDDA & VBAT from 3.3V.
I use an external voltage reference using LM4121AIM5-ADJ which generates 3V from 3.3V input.
When I use this external reference of 3V as VREF+, I would like to understand whether the ADC input range Vain can still be in the range of 0 to VDDA (i.e., 3.3V). Please advice whether the ADC input upto 3.3V is fine or will it cause any issue/damage to the STM32 MCU when VREF+ is 3V.
Looking forward for your immediate support in this regard.
Regards,
Sridevi