Skip to main content
Associate III
May 16, 2024
Question

STM32F407 using advanced timer TIM1 in output compare

I have been unsuccessful in using TIM1 in Output Compare mode. I was trying to use the code that works for the general purpose timers but I cannot get it to work with the advanced timer TIM1. I read online that it is because it was an advanced timer and I had to set the TIMx_BDTR.MOE bit. I have tried this but am still not seeing the signal on my oscilloscope although I can see it for the general purpose timers expected.

 

void TIMER1_Init()
{
 TIM_OC_InitTypeDef tim1OC_init;
 GPIO_InitTypeDef gpio_init;

 // Enable the TIM1 clock
 __HAL_RCC_TIM1_CLK_ENABLE();

 // Enable the GPIO clock for TIM1 channel pin (e.g., PA8 for TIM1_CH1)
 __HAL_RCC_GPIOA_CLK_ENABLE();

 // Configure GPIO pin for TIM1_CH1
 gpio_init.Pin = GPIO_PIN_8;
 gpio_init.Mode = GPIO_MODE_AF_PP;
 gpio_init.Pull = GPIO_NOPULL;
 gpio_init.Speed = GPIO_SPEED_FREQ_LOW;
 gpio_init.Alternate = GPIO_AF1_TIM1;
 HAL_GPIO_Init(GPIOA, &gpio_init);

 // Enable the Main Output (MOE) for advanced timers
 TIM1->BDTR |= TIM_BDTR_MOE;

 // Initialize TIM1 base
 htimer1.Instance = TIM1;
 htimer1.Init.Prescaler = 1;
 htimer1.Init.Period = 0xFFFF;
 if (HAL_TIM_OC_Init(&htimer1) != HAL_OK)
 {
 Error_handler();
 }

 // Configure Output Compare mode for TIM1_CH1
 tim1OC_init.OCMode = TIM_OCMODE_TOGGLE;
 tim1OC_init.OCPolarity = TIM_OCPOLARITY_HIGH;
 tim1OC_init.Pulse = pulse[4];

 if (HAL_TIM_OC_ConfigChannel(&htimer1, &tim1OC_init, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_handler();
 }
}

 

 

Note: I am using function HAL_TIM_OC_Start_IT(&htimer1, TIM_CHANNEL_1) != HAL_OK

 

 

 

 

This topic has been closed for replies.

1 reply

ST Employee
May 20, 2024

Hello @jlaufer, 

Have you checked the state of the register, TIM1's CCR1, SR, and DIER to ensure they are set correctly? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.