Skip to main content
kyouma001
Associate II
January 27, 2023
Solved

STM32F407 Timer does not work

  • January 27, 2023
  • 3 replies
  • 1374 views

Hi I am trying to initialize TIM2 to get a PWM outpt from PA15 of my STM32F407 development board. Here is my TIM init function:

void TIMConfig (void) {
	/*************>>>>>>> STEPS FOLLOWED <<<<<<<<************
	1. Enable the TIM2 clock
	2. Set clock division, enable auto-reload preload
	3. 
	********************************************************/
	
	//	1. Enable the TIM2 clock
	RCC->APB1ENR 	|=	RCC_APB1ENR_TIM2EN;
	
	//	2. Set clock coeff. as 2, enable auto-reload preload
	TIM2->CR1		= 	TIM_CR1_CKD_0 | TIM_CR1_ARPE | TIM_CR1_CMS_0;
	//TIM2->DIER		|= 	TIM_DIER_UIE;
	
	TIM2->CNT		=	0;
	
	TIM2->PSC		=	(uint32_t) 0;
	TIM2->ARR		= 	(uint32_t) 8400;
	
	TIM2->CCR1		= 	(uint32_t) 840;
	TIM2->RCR		= 	(uint32_t) 0;
	
	TIM2->CCMR1		=	TIM_CCMR1_OC1PE | TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_0;	 
	TIM2->CCER		=	TIM_CCER_CC1E | TIM_CCER_CC1P;
	
	TIM2->CR1		|=	TIM_CR1_CEN;
}

And GPIO config function:

void GPIOConfig (void) {
	/*************>>>>>>> STEPS FOLLOWED <<<<<<<<************
	1. Enable the GPIO clock
	2. Set the pin modes
	3. Configure the output mode
	********************************************************/
	
	//	1. Enable the GPIO clock
	RCC->AHB1ENR	|= 	RCC_AHB1ENR_GPIODEN | RCC_AHB1ENR_GPIOAEN;
	
	//	2. Set the pin modes
	//		D13 as output
	GPIOD->MODER	|= 	GPIO_MODER_MODE13_0;
	//		A15 as alternate function
	GPIOA->MODER	|=	GPIO_MODER_MODE15_1;
	GPIOA->AFR[1]	|=	GPIO_AFRH_AFSEL15_0;
	
	//	3. Configure the output mode
	GPIOD->OTYPER	|= 	0;
	GPIOD->OSPEEDR	|= 	0;
}

I call these 2 function in main but I can not see the PWM signal on PA15 pin. What is my fault? Thanks in advance.

This topic has been closed for replies.
Best answer by waclawek.jan

As you set TIMx_CR1.ARPE, the first cycle until the first update takes the original ARR value, ie. 0xFFFF'FFFF timer clocks.

JW

3 replies

waclawek.jan
waclawek.janBest answer
Super User
January 27, 2023

As you set TIMx_CR1.ARPE, the first cycle until the first update takes the original ARR value, ie. 0xFFFF'FFFF timer clocks.

JW

kyouma001
kyouma001Author
Associate II
January 29, 2023

Thanks this worked for me.

S.Ma
Principal
January 28, 2023

In this example, LED Dimming by PWM. (LEDs.c)