Associate
March 4, 2019
Question
STM32F407 Timer->DMA->GPIO
- March 4, 2019
- 3 replies
- 1361 views
Hello
I'm trying to use DMA to directly write on GPIO port, and I've attached the code snippet I'm using to do so.
But, I'm getting this exception which is stopping the DMA and fails writing data.
Any thoughts?
Regards.
GPIO Init:
__HAL_RCC_GPIOD_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
/*Configure GPIO pins : PD12 PD13 PD14 PD15 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);TIM6 Init:
void MX_TIM6_Init(void)
{
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim6.Instance = TIM6;
htim6.Init.Prescaler = 79;
htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
htim6.Init.Period = 99;
if (HAL_TIM_Base_Init(&htim6) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}DMA Init:
void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
if(htim_base->Instance==TIM6)
{
/* Peripheral clock enable */
__HAL_RCC_TIM6_CLK_ENABLE();
/* TIM6 DMA Init */
/* TIM6_UP Init */
hdma_tim6_up.Instance = DMA1_Stream1;
hdma_tim6_up.Init.Channel = DMA_CHANNEL_7;
hdma_tim6_up.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tim6_up.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim6_up.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim6_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_tim6_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_tim6_up.Init.Mode = DMA_CIRCULAR;
hdma_tim6_up.Init.Priority = DMA_PRIORITY_HIGH;
hdma_tim6_up.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_tim6_up) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim6_up);
}
}Start Transfer:
uint32_t blink_led[2] = {
(uint32_t)GPIO_PIN_13, // bit = 0
(uint32_t)GPIO_PIN_13 << 16 // bit = 1
};
void DMA_Start_Transfer(void) {
HAL_DMA_Start_IT(htim6.hdma[TIM_DMA_ID_UPDATE], (uint32_t)&blink_led, (uint32_t)&GPIOD->BSRR, 2);
__HAL_TIM_ENABLE_DMA(&htim6, TIM_DMA_UPDATE);
__HAL_TIM_ENABLE(&htim6);
}