Skip to main content
Associate II
June 24, 2024
Solved

STM32F407 PWM output not stable

I am trying to set up PWM on Channel 1, 2, 3 of TIM3. At first I set up only Channel 1 and the output voltage of PWM is 2.8V. But after I set up the other two channels, the output voltage of Channel 1 & 3 gets to 3.6V, while that of Channel 2 is still 2.8V. Here is the GPIO and TIM settings of TIM and PWM:

void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOF_CLK_ENABLE();

__HAL_RCC_GPIOH_CLK_ENABLE();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

/*Configure GPIO pin Output Level */

// HAL_GPIO_WritePin(GPIOF, GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8, GPIO_PIN_RESET);

/*Configure GPIO pins : PF6 PF7 PF8 */

GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

/*Configure GPIO pin : PA6 PA7 */

GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/*Configure GPIO pin : PB0 */

GPIO_InitStruct.Pin = GPIO_PIN_0;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

}
TIM_HandleTypeDef htim3;
static void TIM_Mode_Config() {

TIM_OC_InitTypeDef sConfigOC;

ADV_TIM_CLK_ENABLE();

// Set TIM3 for all channels.

htim3.Instance = ADV_TIM;

// TIM3 clock freq = 84MHz

// TIM3 actual freq = 84MHz / 84 = 1MHz

htim3.Init.Prescaler = ADV_TIM_PRESCALER - 1;

// PWM freq = 1MHz / 1000 = 1kHz

htim3.Init.Period = ADV_TIM_PERIOD - 1;

htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;

HAL_TIM_Base_Init(&htim3);

HAL_TIM_PWM_Init(&htim3);

// Set PWM

sConfigOC.OCMode = TIM_OCMODE_PWM1;

// Duty = 50%

sConfigOC.Pulse = ADV_TIM_DEFAULT_PULSE;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1);

HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2);

HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_2);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_3);

}

Any help will be highly appreciated. Thank you all.

This topic has been closed for replies.
Sarra.SBest answer
ST Employee
August 1, 2024

Hello @LittleYe233, sorry for the delayed answer, 

Your code seems ok, is it a custom board? maybe it's a hardware connections issue 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Sarra.SBest answer
ST Employee
August 1, 2024

Hello @LittleYe233, sorry for the delayed answer, 

Your code seems ok, is it a custom board? maybe it's a hardware connections issue 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
August 28, 2024

Thank you. It is a custom board indeed. I will try to find out what the hardware issue is.