STM32F407 MCO with HSE source no output
I am using an 8MHz crystal HSE, and the application (MBED) is able to use CAN, USB, UART, etc properly, so the timing for the HSE is setup correctly. When I try to use the HSE as a source for MCO1 or MCO2 however, it does not work, I get no output. If I use the HSI on MCO1 or the PLLCLK on MCO2, I get the expected frequencies, but nothing on HSE. I am using an ABM3B-8.000MHZ-10-1-U-T (10pF) crystal with 15pF load caps, is that relevant at all?