Skip to main content
nagano
Associate II
Jun 1, 2015 1:55 AM UTC
Question

STM32F407 JTAG and Flash Loader Demonstrator Unsuccessful

Posted on June 01, 2015 at 03:55

I have serious problem.

I tried to write software to the devices with JTAG and Flash Loader Demonstrator,but both of them could not find device.

I guess the device revision has something different with revision ''Z''.

Revision ''Z'' devices are successful with JTAG and Flash Loader Demonstrator,

however ''L'' are unsuccessful at all.

If anyone know about this problem, please tell me tips.

Following infomation was tried to write with JTAG and Flash Loader Demonstrator.

--- Unsuccessful Device BGA Package---

ARM L

STM32

F407IEH6

HPADX VQ

KOR HP 504

--- Successful Device 1. BGA Package---

ARM Z

STM32

F407IEH6

HPAFW VG

KOR HP 322

--- Successful Device 2. QFP Package---

ST Z

STM32F407ZGT6

ARM HPABUVG

KORHP4L7

    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    Jun 1, 2015 3:28 AM UTC
    Posted on June 01, 2015 at 05:28

    No particular insight.

    Usual things to confirm :

    Voltages on VCAP pins

    State of NRST pin

    State of BOOTx pins

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    nagano
    naganoAuthor
    Associate II
    Jun 1, 2015 3:34 AM UTC
    Posted on June 01, 2015 at 05:34

    Thank you, clive1

    I rework device revision L to Z then the MPU connect with JTAG and Serial.(On some of same PCB bords.)

    So I worder why doesn't work this device.

    Everything same as revision L.

    nagano
    naganoAuthor
    Associate II
    Jun 1, 2015 4:06 AM UTC
    Posted on June 01, 2015 at 06:06

    Hi, clive1

     

    >Voltages on VCAP pins

    Should I connect BYPASS_REG pin to Low?

    Now, this pin is open.

    nagano
    naganoAuthor
    Associate II
    Jun 8, 2015 7:16 AM UTC
    Posted on June 08, 2015 at 09:16

    As the result, VCAP Pins Voltage is a Key!

    Bypass_REG pin connect to the GND throuh 10k ohm, then

    Voltage on VCAP is about 2.6V and confirm to write firmware.

    Now, Everything is OK.

    Thank you a lot.

    Tesla DeLorean
    Guru
    Jun 8, 2015 1:25 PM UTC
    Posted on June 08, 2015 at 15:25

    Shouldn't the VCAP pins be at 1.25V?! How have you got these parts wired up? (schematic)

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    nagano
    naganoAuthor
    Associate II
    Jun 9, 2015 1:43 AM UTC
    Posted on June 09, 2015 at 03:43

    Hello Clive

    >Shouldn't the VCAP pins be at 1.25V?! How have you got these parts wired up? >(schematic)

    It was 1.25V. I made typo.

    Thanks.