Skip to main content
hakand
Associate
Jun 19, 2019 12:05 PM UTC
Solved

STM32F407 I2C1 EV and ER Interrupt Problem

Hello Everyone,

I have dealing with STM32F407 I2C peripheral in order to implement Non-blocking communication.

I have made many trials but I2C1 event and error interrupts never occur. I checked the SB bits during the debug mode it becomes 1,the other register seems okay but interrupt is never created. Also I have made different trials, changed interrupt priorities, enabled  ev and er interrupts before enabling the periheral, after enabling periheral and after start condition is generated.

I have made other trials with cubemx and hal library for my board. After SB bit is set interrupt occured. However  I couldn’t see the start bit  from logic analyzer.

What am I missing here ?

I am using IAR 8.32, Here is my code ;

I2C.c
void I2C1_SystemInit(void ){
 I2C1->CR1 &= ~I2C_CR1_PE; // I2C peripheral disable 
 // I2C1 Initialization PB8 (SCL) ve PB9 (SDA) 
 RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIOB
 GPIOB->AFR[1] |= (4); // PB8 AF4 for I2C1
 GPIOB->AFR[1] |= (4 << 4); // PB9 AF4 for I2C1 
 GPIOB->MODER &= ~(3 << 16);	 // Clear bits 12 & 13 (PB8)
 GPIOB->MODER |= GPIO_MODER_MODER8_1;	 // Set GPIOB8 to alternate function 
 GPIOB->MODER &= ~(3 << 18);	 // Clear bits 14 & 15 (PB9)
 GPIOB->MODER |= GPIO_MODER_MODER9_1;	 // Set GPIOB9 to alternate function 
 GPIOB->OTYPER |= GPIO_OTYPER_OT_8;	 // Open Drain
 GPIOB->OTYPER |= GPIO_OTYPER_OT_9; // Open Drain
 GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0;	 // Pull-Up
 GPIOB->PUPDR |= GPIO_PUPDR_PUPDR9_0;	 // Pull-Up
 GPIOB->OSPEEDR |= (3<<16);
 GPIOB->OSPEEDR |= (3<<18);
 RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; // Enable clock for I2C1
 I2C1->CR2 |= 0x14; 
 I2C1->CCR |= 208; 
 I2C1->TRISE |= 0x5; // 100 kHz
// I2C1->CR1 |= I2C_CR1_NOSTRETCH;
// I2C1->CR1 |= I2C_CR1_ACK; // Acknowledge enable 
// I2C1->CR1 &= ~I2C_CR1_POS; // Disable Pos 
 // I2C1->CR2 |= I2C_CR2_ITEVTEN; //<Event Interrupt Enable 
 // I2C1->CR2 |= I2C_CR2_ITBUFEN; //<Buffer Interrupt Enable 
 // I2C1->CR2 |= I2C_CR2_ITERREN;
 I2C1->CR1 |= I2C_CR1_PE;
}
void I2C1_EV_IRQHandler(void){ 
 flag=1; uint32_t sr2itflags = (I2C1->SR2);
 uint32_t sr1itflags = (I2C1->SR1);
 uint32_t itsources = (I2C1->CR2); }
void I2C1_ER_IRQHandler(void){ flag=2; uint32_t sr2itflags = (I2C1->SR2);
 uint32_t sr1itflags = (I2C1->SR1);
 uint32_t itsources = (I2C1->CR2); }
 
Main.c
void Init_Priorities(void){
 SCB->AIRCR = ((uint32_t)0x05FA0000) | NVIC_PriorityGroup_4; // NVIC_SetPriorityGrouping(4)
 NVIC_SetPriority(TIM1_UP_TIM10_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0)); 
 NVIC_SetPriority(ADC_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),1, 0)); 
 NVIC_SetPriority(TIM1_BRK_TIM9_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),2, 0)); 
 NVIC_SetPriority(TIM1_TRG_COM_TIM11_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),3, 0)); 
 NVIC_SetPriority(TIM8_BRK_TIM12_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),4, 0)); 
 NVIC_SetPriority(TIM8_TRG_COM_TIM14_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0)); 
 NVIC_SetPriority(I2C1_EV_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),6, 0)); 
 NVIC_SetPriority(I2C1_ER_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),7, 0)); 
 NVIC_SetPriority(I2C2_EV_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),8, 0)); 
 NVIC_SetPriority(I2C2_ER_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),9, 0)); 
}
 
void TIM8_TRG_COM_TIM14_IRQHandler(void) { RD_EEP1(); TIM14->SR &= ~(TIM_SR_UIF); } 
void RD_EEP1(void){ 
 if((I2C1->CR1 & I2C_CR1_PE) != I2C_CR1_PE){
 I2C1->CR1 |= I2C_CR1_PE; } // I2C peripheral enable
 
 I2C1->CR1 &= ~I2C_CR1_POS;
 I2C1->CR1 |= I2C_CR1_START; asm("nop"); asm("nop"); asm("nop");
 I2C1->CR2 |= I2C_CR2_ITEVTEN; //<Event Interrupt Enable 
 I2C1->CR2 |= I2C_CR2_ITBUFEN; //<Buffer Interrupt Enable 
 I2C1->CR2 |= I2C_CR2_ITERREN;
 GREEN_LED_ON;
}
 
 int main()
 { for(uint16_t i=0;i<10000;i++); // wait for a while K
 Fan_Control(); // Fan pins initilization
 init_inj_adc_interrupt(); // ADC Injected Channel 
 I2C1_SystemInit();
 DAC1_Init();
 TIM9_Init(); // 1mS Timer Interrupt Init 
 TIM11_Init(); // 10mS Timer Interrupt Init 
 TIM12_Init(); // 100mS Timer Interrupt Init 
 TIM14_Init(); // 1000mS Timer Interrupt Init 
 Init_Priorities();
 while(1){ 
 } }
 
 

This topic has been closed for replies.
hakand
hakandBest answer
Associate
Jun 20, 2019 7:58 AM UTC

Hello again, I found the problem guys,

change the code like this ;

void I2C1_SystemInit(void ){
 // I2C1 Initialization PB8 (SCL) ve PB9 (SDA) 
 RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIOB
 GPIOB->AFR[1] |= (4); // PB8 AF4 for I2C1
 GPIOB->AFR[1] |= (4 << 4); // PB9 AF4 for I2C1 
 GPIOB->MODER &= ~(3 << 16);	 // Clear bits 12 & 13 (PB8)
 GPIOB->MODER |= GPIO_MODER_MODER8_1;	 // Set GPIOB8 to alternate 
 GPIOB->MODER &= ~(3 << 18);	 // Clear bits 14 & 15 (PB9)
 GPIOB->MODER |= GPIO_MODER_MODER9_1;	 // Set GPIOB9 to alternate
 GPIOB->OTYPER |= GPIO_OTYPER_OT_8;	
 GPIOB->OTYPER |= GPIO_OTYPER_OT_9; 
 GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0;	 // pull-up, 
 GPIOB->PUPDR |= GPIO_PUPDR_PUPDR9_0;	 // pull-up, 
 GPIOB->OSPEEDR |= (3<<16);
 GPIOB->OSPEEDR |= (3<<18);
 RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; // Enable clock for I2C1
 while(!(RCC->APB1ENR & RCC_APB1ENR_I2C1EN) ){} 
 for(uint16_t i=0;i<1000;i++); 
 NVIC_SetPriority(I2C1_EV_IRQn, 6);
 NVIC_EnableIRQ(I2C1_EV_IRQn);
 NVIC_SetPriority(I2C1_ER_IRQn, 7);
 NVIC_EnableIRQ(I2C1_ER_IRQn);
 I2C1->CR1 &= ~I2C_CR1_PE; // I2C peripheral disable 
 I2C1->CR2 |= 0x2A; //0x14; 
 I2C1->CCR |= 0X0D2; //208; 
 I2C1->TRISE |= 0x2B; //0x5; 
 I2C1->CR1 |= I2C_CR1_PE;
 for(uint16_t i=0;i<1000;i++); 
} 

1 reply

hakand
hakandAuthorBest answer
Associate
Jun 20, 2019 7:58 AM UTC

Hello again, I found the problem guys,

change the code like this ;

void I2C1_SystemInit(void ){
 // I2C1 Initialization PB8 (SCL) ve PB9 (SDA) 
 RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIOB
 GPIOB->AFR[1] |= (4); // PB8 AF4 for I2C1
 GPIOB->AFR[1] |= (4 << 4); // PB9 AF4 for I2C1 
 GPIOB->MODER &= ~(3 << 16);	 // Clear bits 12 & 13 (PB8)
 GPIOB->MODER |= GPIO_MODER_MODER8_1;	 // Set GPIOB8 to alternate 
 GPIOB->MODER &= ~(3 << 18);	 // Clear bits 14 & 15 (PB9)
 GPIOB->MODER |= GPIO_MODER_MODER9_1;	 // Set GPIOB9 to alternate
 GPIOB->OTYPER |= GPIO_OTYPER_OT_8;	
 GPIOB->OTYPER |= GPIO_OTYPER_OT_9; 
 GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0;	 // pull-up, 
 GPIOB->PUPDR |= GPIO_PUPDR_PUPDR9_0;	 // pull-up, 
 GPIOB->OSPEEDR |= (3<<16);
 GPIOB->OSPEEDR |= (3<<18);
 RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; // Enable clock for I2C1
 while(!(RCC->APB1ENR & RCC_APB1ENR_I2C1EN) ){} 
 for(uint16_t i=0;i<1000;i++); 
 NVIC_SetPriority(I2C1_EV_IRQn, 6);
 NVIC_EnableIRQ(I2C1_EV_IRQn);
 NVIC_SetPriority(I2C1_ER_IRQn, 7);
 NVIC_EnableIRQ(I2C1_ER_IRQn);
 I2C1->CR1 &= ~I2C_CR1_PE; // I2C peripheral disable 
 I2C1->CR2 |= 0x2A; //0x14; 
 I2C1->CCR |= 0X0D2; //208; 
 I2C1->TRISE |= 0x2B; //0x5; 
 I2C1->CR1 |= I2C_CR1_PE;
 for(uint16_t i=0;i<1000;i++); 
}